Hello,
We are currently working on an energy monitoring device which is implemented with an ADE9000.
During the qualification of the product under different temperature conditions, we experienced precision drifts at negative temperatures for V, I, and consequently P, as shown below:
| injected | -5°C | Errors | ||||||||||
| V1 (V) | I1 (A) | PF | P1 th (W) | measured V1 (V) | Measured Current I1 (A) | measured Power P1 (W) | absolute drift V1 (V) | Relative Err V1 | absolute drift I1 (mA) | Relative Error I1 | Absolute error P1 (W) | Relative Power Error |
| 230 | 10,00 | 1 | 2300,000 | 229,62 | 9,9907 | 2293,01 | -0,38 | -0,17% | -9,3000 | -0,09% | -6,99 | -0,30% |
| 230 | 5,00 | 1 | 1150,000 | 229,62 | 4,9957 | 1146,59 | -0,38 | -0,17% | -4,3000 | -0,09% | -3,41 | -0,30% |
| 230 | 2,50 | 1 | 575,000 | 229,63 | 2,4981 | 573,36 | -0,37 | -0,16% | -1,9000 | -0,08% | -1,64 | -0,29% |
| 230 | 1,00 | 1 | 230,000 | 229,63 | 0,9992 | 229,34 | -0,37 | -0,16% | -0,8000 | -0,08% | -0,66 | -0,29% |
| 230 | 0,50 | 1 | 115,000 | 229,63 | 0,4996 | 114,66 | -0,37 | -0,16% | -0,4000 | -0,08% | -0,34 | -0,30% |
| 230 | 0,25 | 1 | 57,500 | 229,63 | 0,2499 | 57,34 | -0,37 | -0,16% | -0,1000 | -0,04% | -0,16 | -0,28% |
-> we can see what looks like an offset in the voltage measurement, do you have any explanation for this?
1- As a first step, we mounted 25 ppm resistors and then 10 ppm resistors for voltage channels, without improvement.
2- After that, we monitored the input voltage at the entry of the ADE9000 on channel V2, and we didn't get a real difference or drift after the resistor divider stage.
3- Also, we measured the internal 1.2V Vref, and we didn't see a large drift: Vref = 1.2556V @ 23°C and Vref = 1.2561V @ -5°C -> 11 ppm/°C.
Now we aim to integrate drift and gain compensation over temperature, as mentioned in the datasheet.
Is it possible to determine the drift profile of the ADE9000 in our hardware implementation?
Can we determine a general compensation factor based on experimental tests, rather than requiring calibration for each product?
Thanks,