Post Go back to editing

Need help on Update File Path for maxim.mk in no-OS

Thread Summary

The user encountered an error while building a project for the AD-PQMON-SL using the Maxim SDK October 2024 release. The error was due to a missing `arm-none-eabi-gcc` compiler. The final solution was to revert changes made to `maxim.mk` as these are not necessary for the October 2024 release. The user can verify the SDK version by checking for updates via the Maintenance Tool or by cloning the MSDK repository and switching to the `v2024_10` tag.
AI Generated Content
Category: Hardware
Product Number: AD-PQMON-SL

Hardware: AD-PQMON-SL

 

Software: Maxim SDK October Release 2024

 

Error Message in Git Bash:

YongYH@YongYH-Laptop MINGW64 ~
$ cd /c/Users/YongYH/no-OS/projects/eval-pqmon && ./build_hex.sh
[INFO] Cleaning previous build...
Using USB as interface for IIO communication
find: ‘C:/MaximSDK/Libraries/../../../Tools/gcc/arm-none-eabi’: No such file or directory
which: no arm-none-eabi-gcc in (/c/Users/YongYH/bin:/mingw64/bin:/usr/local/bin:/usr/bin:/usr/bin:/mingw64/bin:/usr/bin:/c/Users/YongYH/bin:/c/Windows/system32:/c/Windows:/c/Windows/System32/Wbem:/c/Windows/System32/WindowsPowerShell/v1.0:/c/Windows/System32/OpenSSH:/c/Users/ChooYC/AppData/Local/Programs/Python/Python311/Scripts:/c/Program Files/PuTTY:/cmd:/c/Program Files/MongoDB/Server/6.0/bin:/c/Program Files/mongosh-1.8.0-win32-x64/bin:/c/Python27:/c/MinGW/bin:/c/ProgramData/chocolatey/bin:/c/Python/Python311/Scripts:/c/Program Files/PowerShell/7-preview/preview:/c/Program Files (x86)/Windows Kits/10/Windows Performance Toolkit:/c/Program Files/PowerShell/7:/c/Program Files/PVsyst8.0.17:/c/Users/YongYH/AppData/Local/Programs/Python/Python310/Scripts:/c/Users/YongYH/AppData/Local/Programs/Python/Python310:/c/Users/YongYH/AppData/Local/Microsoft/WindowsApps:/c/Users/ChooYC/AppData/Local/Programs/Python/Python311:/c/Users/ChooYC/AppData/Local/Programs/Python/Python311/Scripts:/usr/bin/vendor_perl:/usr/bin/core_perl)
which: no arm-none-eabi-gcc in (/c/Users/YongYH/bin:/mingw64/bin:/usr/local/bin:/usr/bin:/usr/bin:/mingw64/bin:/usr/bin:/c/Users/YongYH/bin:/c/Windows/system32:/c/Windows:/c/Windows/System32/Wbem:/c/Windows/System32/WindowsPowerShell/v1.0:/c/Windows/System32/OpenSSH:/c/Users/ChooYC/AppData/Local/Programs/Python/Python311/Scripts:/c/Program Files/PuTTY:/cmd:/c/Program Files/MongoDB/Server/6.0/bin:/c/Program Files/mongosh-1.8.0-win32-x64/bin:/c/Python27:/c/MinGW/bin:/c/ProgramData/chocolatey/bin:/c/Python/Python311/Scripts:/c/Program Files/PowerShell/7-preview/preview:/c/Program Files (x86)/Windows Kits/10/Windows Performance Toolkit:/c/Program Files/PowerShell/7:/c/Program Files/PVsyst8.0.17:/c/Users/YongYH/AppData/Local/Programs/Python/Python310/Scripts:/c/Users/YongYH/AppData/Local/Programs/Python/Python310:/c/Users/YongYH/AppData/Local/Microsoft/WindowsApps:/c/Users/ChooYC/AppData/Local/Programs/Python/Python311:/c/Users/ChooYC/AppData/Local/Programs/Python/Python311/Scripts:/usr/bin/vendor_perl:/usr/bin/core_perl)
which: no arm-none-eabi-gcc in (/c/Users/YongYH/bin:/mingw64/bin:/usr/local/bin:/usr/bin:/usr/bin:/mingw64/bin:/usr/bin:/c/Users/YongYH/bin:/c/Windows/system32:/c/Windows:/c/Windows/System32/Wbem:/c/Windows/System32/WindowsPowerShell/v1.0:/c/Windows/System32/OpenSSH:/c/Users/ChooYC/AppData/Local/Programs/Python/Python311/Scripts:/c/Program Files/PuTTY:/cmd:/c/Program Files/MongoDB/Server/6.0/bin:/c/Program Files/mongosh-1.8.0-win32-x64/bin:/c/Python27:/c/MinGW/bin:/c/ProgramData/chocolatey/bin:/c/Python/Python311/Scripts:/c/Program Files/PowerShell/7-preview/preview:/c/Program Files (x86)/Windows Kits/10/Windows Performance Toolkit:/c/Program Files/PowerShell/7:/c/Program Files/PVsyst8.0.17:/c/Users/YongYH/AppData/Local/Programs/Python/Python310/Scripts:/c/Users/YongYH/AppData/Local/Programs/Python/Python310:/c/Users/YongYH/AppData/Local/Microsoft/WindowsApps:/c/Users/ChooYC/AppData/Local/Programs/Python/Python311:/c/Users/ChooYC/AppData/Local/Programs/Python/Python311/Scripts:/usr/bin/vendor_perl:/usr/bin/core_perl)

Maxim.mk:

Updated based on (+) Fail to use the function max31343_reg_read_time_stamp() - Q&A - Energy - EngineerZone

diff --git a/tools/scripts/maxim.mk b/tools/scripts/maxim.mk
index 434ac812..5199a93a 100644
--- a/tools/scripts/maxim.mk
+++ b/tools/scripts/maxim.mk
@@ -15,7 +15,7 @@ OC=arm-none-eabi-objcopy
 SIZE=arm-none-eabi-size
 
 PYTHON = python
-ARM_COMPILER_PATH = $(realpath $(dir $(shell find $(MAXIM_LIBRARIES)/../Tools/GNUTools -wholename "*bin/$(CC)" -o -name "$(CC).exe")))
+ARM_COMPILER_PATH = $(realpath $(dir $(shell find $(MAXIM_LIBRARIES)/../../../Tools/gcc/arm-none-eabi -wholename "*bin/$(CC)" -o -name "$(CC).exe")))
 
 # Use the user provided compiler if the SDK doesn't contain it.
 ifeq ($(ARM_COMPILER_PATH),)
@@ -51,6 +51,11 @@ include $(MAXIM_LIBRARIES)/CMSIS/Device/Maxim/$(TARGET_UCASE)/Source/GCC/$(TARGE
 endif
 include $(MAXIM_LIBRARIES)/PeriphDrivers/$(TARGET_LCASE)_files.mk
 
+PERIPH_DRIVER_C_FILES += $(SOURCE_DIR)/SYS/mxc_assert.c
+PERIPH_DRIVER_C_FILES += $(SOURCE_DIR)/SYS/mxc_delay.c
+PERIPH_DRIVER_C_FILES += $(SOURCE_DIR)/SYS/nvic_table.c
+PERIPH_DRIVER_C_FILES += $(SOURCE_DIR)/SYS/mxc_lock.c
+
 HEX=$(basename $(BINARY)).hex
 TARGET_REV=0x4131
 

Troubleshooting Step that I have taken:

  • File path in Windows: C:\MaximSDK\Tools\GNUTools\10.3\lib\gcc\arm-none-eabi
  • Update to ARM_COMPILER_PATH = $(MAXIM_LIBRARIES)/Tools/GNUTools/10.3/lib/gcc/arm-none-eabi
  • But there's new error message

YongYH@YongYH-Laptop MINGW64 ~
$ cd /c/Users/YongYH/no-OS/projects/eval-pqmon && ./build_hex.sh
[INFO] Cleaning previous build...
Using USB as interface for IIO communication
[14:09:53] [Delete] C:/Users/YongYH/no-OS/projects/eval-pqmon/build
[INFO] Building new HEX...
Using USB as interface for IIO communication
[14:09:55] Building for maxim
Using USB as interface for IIO communication
[14:09:58] Building for target max32650
[14:09:58] Creating IDE project
Using USB as interface for IIO communication
Using USB as interface for IIO communication
[14:11:37] Generating build flags
[14:11:45] Creating symlinks to source files
Using USB as interface for IIO communication
[14:11:49] [CC] heap.c
process_begin: CreateProcess(NULL, arm-none-eabi-gcc -c @C:/Users/YongYH/no-OS/projects/eval-pqmon/build/eval-pqmon-cflags.txt C:/Users/YongYH/no-OS/projects/eval-pqmon/build/app/root/MaximSDK/Libraries/CMSIS/Device/Maxim/MAX32650/Source/heap.c -o C:/Users/YongYH/no-OS/projects/eval-pqmon/build/objs/eval-pqmon/build/app/root/MaximSDK/Libraries/CMSIS/Device/Maxim/MAX32650/Source/heap.o, ...) failed.
make (e=2): The system cannot find the file specified.
make[1]: *** [../../tools/scripts/generic.mk:289: C:/Users/YongYH/no-OS/projects/eval-pqmon/build/objs/eval-pqmon/build/app/root/MaximSDK/Libraries/CMSIS/Device/Maxim/MAX32650/Source/heap.o] Error 2
make: *** [../../tools/scripts/generic.mk:268: all] Error 2
[ERROR] HEX file not found: /c/Users/YongYH/no-OS/projects/eval-pqmon/build/eval-pqmon.hex

  • Hi. ,  since you are using the October 2024 release you don't need to make any modifications to maxim.mk. Those changes are only needed when building against the latest MSDK cloned from git (where the directory structure changed). Please revert your changes to maxim.mk and the build should work.

  • Hi  , how to check whether my Maxim SDK version is October 2024 release? because i'm using online installer MaximMicrosSDK_win.exe.

    If I'm using offline installer MaximMicrosSDK_OFFLINE_2024_10_Windows.zip, will pop out error.

  • Hi,

    Regarding the offline installer, it seems there is an issue specifically with the MaximMicrosSDK_OFFLINE_2024_10_Windows.zip.

    As for checking your SDK version: I don't think there is a way to check the specific release you are running if you use the online installer. But when using the online installer, in the installation folder you should find a Maintenance Tool application. Run it and select "Update Components". If it says that there are no updates available, you have the latest release.

    Alternatively, you can clone the MSDK repository directly, which gives you full control over the release versions following these steps:

    1. Follow the steps from the link for Cloning and Toolchain Setup: msdk/README.md at main · analogdevicesinc/msdk
    2. Open a terminal in the cloned MSDK folder
    3. Run git tag to list all available releases
    4. Switch to a specific release with: git checkout v2024_10