Hardware: AD-PQMON-SL
Goal:
Display RTC clock time (with battery) in iio_pqm.c
max31343_reg_read_time_stamp(max31343_dev, &ts) case CURRENT_TIME_READABLE: return snprintf(buf, len, "%04d-%02d-%02d %02d:%02d:%02d", ts.year, ts.mon + 1, ts.day, ts.hr, ts.min, ts.sec);
Problem Description:
After adding max31343 initialisation, set the timestamp and cleanup code in basic_example.c, a hex file can be built, but fails to be detected by iio_info
Microsoft Windows [Version 10.0.19045.6466] (c) Microsoft Corporation. All rights reserved. C:\Users\YongYH>cd C:\Users\YongYH\Private\Tools\libiio\Windows-VS-2022-x64 & iio_info -u serial:COM4,115200,8n1 Unable to create IIO context serial:COM4,115200,8n1: No such file or directory (2)
Troubleshooting steps that I have taken:
- If max31343 related codes are removed from basic_example.c, iio_info can run without abnormal
- Using latest version of max31343.c and max31343.h
- Tried to refine my code in basic_example.c by using AI, but the error persisted.
/*******************************************************************************
* @file basic_example.c
* @brief PQM firmware, called by main
* @author Robert Budai (robert.budai@analog.com)
********************************************************************************
* Copyright (c) 2024 Analog Devices, Inc.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions are met:
*
* 1. Redistributions of source code must retain the above copyright notice,
* this list of conditions and the following disclaimer.
*
* 2. Redistributions in binary form must reproduce the above copyright notice,
* this list of conditions and the following disclaimer in the documentation
* and/or other materials provided with the distribution.
*
* 3. Neither the name of Analog Devices, Inc. nor the names of its
* contributors may be used to endorse or promote products derived from this
* software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES, INC. “AS IS” AND ANY EXPRESS OR
* IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF
* MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO
* EVENT SHALL ANALOG DEVICES, INC. BE LIABLE FOR ANY DIRECT, INDIRECT,
* INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA,
* OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF
* LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING
* NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*******************************************************************************/
#ifdef BASIC_EXAMPLE
#include "basic_example.h"
#endif
/* ============ ADD THESE INCLUDES AT THE TOP ============ */
#include "max31343.h"
#include "common_data.h"
/* ============ END NEW INCLUDES ============ */
int32_t pqm_init(struct pqm_desc **desc, struct pqm_init_para *param)
{
struct pqm_desc *d;
d = (struct pqm_desc *)no_os_calloc(1, sizeof(*d));
if (!d)
return -ENOMEM;
d->ext_buff = param->ext_buff;
d->ext_buff_len = param->ext_buff_len;
for (int i = 0; i < TOTAL_PQM_CHANNELS; i++) {
for (int j = 0; j < MAX_CH_ATTRS; j++) {
d->pqm_ch_attr[i][j] = 0;
}
}
for (int i = 0; i < PQM_DEVICE_ATTR_NUMBER; i++) {
d->pqm_global_attr[i] = param->dev_global_attr[i];
}
*desc = d;
return 0;
}
int32_t pqm_remove(struct pqm_desc *desc)
{
if (!desc)
return -EINVAL;
no_os_free(desc);
return 0;
}
int32_t update_pqm_channels(void *dev, uint32_t mask)
{
struct pqm_desc *desc;
if (!dev)
return -ENODEV;
desc = dev;
desc->active_ch = mask;
return 0;
}
int32_t close_pqm_channels(void *dev)
{
struct pqm_desc *desc;
if (!dev)
return -ENODEV;
desc = dev;
desc->active_ch = 0;
return 0;
}
#if defined(PQM_CONN_SERIAL)
int32_t enable_RS482_driver()
{
// Enable driver and receiver of ADM2587, used only by serial connection
int status;
struct no_os_gpio_sec *enable_ADM2587;
struct nhd_c12832a1z_dev *nhd_c12832a1z_device;
struct max_gpio_init_param gpio_extra_ip_ADM2587 = {
.vssel = MXC_GPIO_VSSEL_VDDIOH,
};
struct no_os_gpio_init_param gpio_ADM2587_ip = {
.port = 2,
.number = 15,
.pull = NO_OS_PULL_NONE,
.platform_ops = &max_gpio_ops,
.extra = &gpio_extra_ip_ADM2587,
};
status = no_os_gpio_get(&enable_ADM2587, &gpio_ADM2587_ip);
if (status)
return status;
status = no_os_gpio_set_value(enable_ADM2587, 1);
return status;
}
#endif
int basic_pqm_firmware()
{
struct no_os_uart_desc *uart_desc;
struct pqm_desc *pqm_desc;
struct iio_app_desc *app;
struct iio_app_init_param app_init_param = {0};
struct iio_data_buffer buff = {
.buff = (void *)iio_data_buffer_loc,
.size = MAX_SIZE_BASE_ADDR_WITH_SIZE,
};
pqlibExample.no_os_cb_desc = NULL;
memset(iio_data_buffer_loc, 0, MAX_SIZE_BASE_ADDR_WITH_SIZE);
int status = SYS_STATUS_SUCCESS;
/* ============ ADD THESE VARIABLE DECLARATIONS ============ */
struct max31343_dev* max31343_dev = NULL;
struct max31343_time_stamp ts;
struct max31343_init_param max31343_init_params;
/* ============ END NEW VARIABLE DECLARATIONS ============ */
status = init_lcd();
if (status)
goto exit;
status = no_os_uart_init(&uart_desc, &uart_ip_stdio);
if (status)
goto exit;
no_os_uart_stdio(uart_desc);
#if defined(PQM_CONN_SERIAL)
status = enable_RS482_driver();
if (status)
goto exit;
#endif
/* ============ INSERT MAX31343 INITIALIZATION HERE ============ */
/* Setup MAX31343 RTC initialization parameters */
max31343_init_params.i2c_init = &i2c_ip;
max31343_init_params.battery_en = 1;
/* Initialize MAX31343 device */
status = max31343_init(&max31343_dev, max31343_init_params);
if (status) {
printf("MAX31343 initialization failed, status: %d\n\r", status);
goto exit;
}
printf("MAX31343 initialized successfully\n\r");
/* Set the time stamp */
ts.sec = 0;
ts.min = 0;
ts.hr = 12;
ts.day = 25;
ts.mon = 2; /* Month: 0-11 (2 = March) */
ts.year = 2026;
status = max31343_set_time_stamp(max31343_dev, ts);
if (status) {
printf("Failed to set time stamp, status: %d\n\r", status);
goto exit;
}
printf("Time stamp set successfully: %02d:%02d:%02d %02d-%02d-%04d\n\r",
ts.hr, ts.min, ts.sec, ts.day, ts.mon + 1, ts.year);
/* ============ END MAX31343 INITIALIZATION ============ */
#if defined(PQM_CONN_T1L)
uint8_t adin1110_mac_address[6] = {0x00, 0x18, 0x80, 0x03, 0x25, 0x60};
struct no_os_gpio_desc *adin1110_swpd_gpio;
struct no_os_gpio_desc *adin1110_tx2p4_gpio;
struct no_os_gpio_desc *adin1110_mssel_gpio;
struct no_os_gpio_desc *adin1110_cfg0_gpio;
struct no_os_gpio_desc *adin1110_cfg1_gpio;
struct no_os_gpio_desc *adin1110_int_gpio;
int ret;
no_os_gpio_get(&adin1110_cfg0_gpio, &adin1110_cfg0_ip);
no_os_gpio_get(&adin1110_swpd_gpio, &adin1110_swpd_ip);
no_os_gpio_get(&adin1110_tx2p4_gpio, &adin1110_tx2p4_ip);
no_os_gpio_get(&adin1110_mssel_gpio, &adin1110_mssel_ip);
no_os_gpio_get(&adin1110_cfg1_gpio, &adin1110_cfg1_ip);
no_os_gpio_get(&adin1110_int_gpio, &adin1110_int_ip);
no_os_gpio_direction_output(adin1110_swpd_gpio, 1);
no_os_gpio_direction_output(adin1110_tx2p4_gpio, 0);
no_os_gpio_direction_output(adin1110_mssel_gpio, 1);
no_os_gpio_direction_output(adin1110_cfg1_gpio, 1);
no_os_gpio_direction_output(adin1110_cfg0_gpio, 1);
no_os_gpio_direction_input(adin1110_int_gpio);
memcpy(adin1110_ip.mac_address, adin1110_mac_address, NETIF_MAX_HWADDR_LEN);
memcpy(app_init_param.lwip_param.hwaddr, adin1110_mac_address,
NETIF_MAX_HWADDR_LEN);
#endif
status = afe_init();
if (status != SYS_STATUS_SUCCESS) {
printf("AFE Init failed \n\r");
goto exit;
}
status = pqm_measurement_init();
if (status != SYS_STATUS_SUCCESS) {
printf("Pqm Measurement Init failed \n\r");
goto exit;
}
status = pqm_init(&pqm_desc, &pqm_ip);
if (status) {
printf("PQM initialization failed \n\r");
goto exit;
}
status = pqm_start_measurement(false);
if (status != SYS_STATUS_SUCCESS) {
printf("PQM could not start measurements, status: %d \n\r", status);
goto exit;
}
printf("Mesurements started \n\r");
struct iio_app_device devices[] = {
IIO_APP_DEVICE("pqm", pqm_desc, &pqm_iio_descriptor, &buff, NULL, NULL)
};
app_init_param.devices = devices;
app_init_param.nb_devices = NO_OS_ARRAY_SIZE(devices);
#if defined(PQM_CONN_USB)
app_init_param.uart_init_params = iio_demo_usb_ip;
#elif defined(PQM_CONN_SERIAL)
app_init_param.uart_init_params = iio_demo_serial_ip;
#elif defined(PQM_CONN_T1L)
app_init_param.uart_init_params = iio_demo_serial_ip;
app_init_param.lwip_param.platform_ops = &adin1110_lwip_ops;
app_init_param.lwip_param.mac_param = &adin1110_ip;
app_init_param.lwip_param.extra = NULL;
#endif
app_init_param.post_step_callback = &(pqm_one_cycle);
status = iio_app_init(&app, app_init_param);
if (status)
goto exit;
status = iio_app_run(app);
iio_app_remove(app);
exit:
/* ============ ADD MAX31343 CLEANUP IN THE EXIT SECTION ============ */
if (max31343_dev) {
int ret_cleanup = max31343_remove(max31343_dev);
if (ret_cleanup) {
printf("MAX31343 removal failed, status: %d\n\r", ret_cleanup);
}
}
/* ============ END MAX31343 CLEANUP ============ */
pqm_remove(pqm_desc);
no_os_uart_remove(uart_desc);
return status;
}