Post Go back to editing

Error returned when trying to read the Power Quality library's "pack" file into the Keil development tool.

Category: Software
Product Number: ADE9430
Software Version: Power Quality Library 1.2.0

We are trying to set up the EVAL-ADE9430 to use the Power Quality library and following the instructions in Section 6.1 of the "ADSW-PQ-CLS Power Quality Library User's Guide".   We are trying to install the Power Quality library's "Pack" file into the Keil tool and getting the following failure (along with a screen capture): 

E: The latest release (0.1.0) in pack's pdsc (AnalogDevices.ADSW-PQ-CLS.pdsc) does not match pack version "1.2.0" 

E: pack version is not the latest in the pdsc file. 

The name of the "pack" file is:  AnalogDevices.ADSW-PQ-CLS.1.2.0.pack

The name of the "pdsc" file is: AnalogDevices.ADSW-PQ-CLS.pdsc

We  are not sure how to get around this, and need help. 

If this requires a newer PQL  library do we need to reapply for it or can we just download it? Thanks 

Parents
  • Hi Mike,

    Thanks for bringing this to our attention.

    We will address the limitations of the two documentation and will upload the update it soon. We are looking to add a quick start guide to the document. 

    Please refer to the FAQ for some common issues and workaround : ADE9430 ADSW-PQ-CLS Power Quality Library Frequently Asked Questions - Documents - Energy - EngineerZone

    Can I please confirm that you are using Keil MDK version 5.34.

    Can you also change the file extension of the .pack file to .zip. After extracting load the .pdsc file directly into Keil.

    As a initial check, please flash the prebuilt .hex file provided within the pack folder. You can use STM32CubeProgrammer version 2.8.0 to flash the .hex file. You can download the cube programmer here : https://www.st.com/en/development-tools/stm32cubeprog.html.

    In the STM32CubeProgrammer window press connect button on the top right using default settings. After Connect turns green, go to the erase and programming window. After selecting the hex file, check the options “Verify Programming” and “Run after programming” and click the “Start Programming” button. Check the Log report for a successful message and a 100% green bar after programming. 

    After the prebuilt .hex file is flashed you can use a terminal emulation tool like Teraterm or Putty to interface with the Board. Please connect using the baud rate mentioned.

    You can try the commands in ADSW-PQ-CLS Power Quality Library User's Guide Pg 35 to verify the PQ Library.

    Regards,

    Aditya

Reply
  • Hi Mike,

    Thanks for bringing this to our attention.

    We will address the limitations of the two documentation and will upload the update it soon. We are looking to add a quick start guide to the document. 

    Please refer to the FAQ for some common issues and workaround : ADE9430 ADSW-PQ-CLS Power Quality Library Frequently Asked Questions - Documents - Energy - EngineerZone

    Can I please confirm that you are using Keil MDK version 5.34.

    Can you also change the file extension of the .pack file to .zip. After extracting load the .pdsc file directly into Keil.

    As a initial check, please flash the prebuilt .hex file provided within the pack folder. You can use STM32CubeProgrammer version 2.8.0 to flash the .hex file. You can download the cube programmer here : https://www.st.com/en/development-tools/stm32cubeprog.html.

    In the STM32CubeProgrammer window press connect button on the top right using default settings. After Connect turns green, go to the erase and programming window. After selecting the hex file, check the options “Verify Programming” and “Run after programming” and click the “Start Programming” button. Check the Log report for a successful message and a 100% green bar after programming. 

    After the prebuilt .hex file is flashed you can use a terminal emulation tool like Teraterm or Putty to interface with the Board. Please connect using the baud rate mentioned.

    You can try the commands in ADSW-PQ-CLS Power Quality Library User's Guide Pg 35 to verify the PQ Library.

    Regards,

    Aditya

Children
  • Dear Aditya,

    Thank you for your response to this. I have a similar issue as Mike. I also followed the instructions in this follow up email with regards to putting the .pdsc file into Keil and I still had no success. what might be the problem. Another question will be, how to make use of user code together with the evaluation version of the PQ library?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.