Hello, I would like to know the common practices for protecting the ADE7758 chip's ADC from ESD events. Which TVS diode is typically used, and where should it be placed—near the chip (1) or near the connector(2), before the voltage divider circuit and the burden resistor circuit?
Is there a need to provide external protection, or is internal ADE ESD protection sufficient?
If external diodes are needed, which diode is suitable? Where should both positions be placed, given that they require different clamping voltages?