Post Go back to editing

Inquiry: Measuring High DC Voltage and Current with ADE7880

Category: Hardware

Good Afternoon,

We are currently utilizing a device from the ADE78xx family for AC power measurements.
While our current focus is on AC, we are interested in extending our measurements to include DC power as well.

I am working on a project that requires measuring high DC voltage and current—specifically around 470 V DC and 2000 A DC.
I would like to understand the feasibility of using the ADE7880 for this purpose.

My questions are:

Can the ADE7880 be used to measure such high DC voltage and current?

Is this approach recommended for achieving accurate DC measurements?

Are there any specific considerations, external circuitry, or precautions required to ensure precise readings at this scale?

Best regards,
Athul E

Parents
  • In theory disabling the high pass filter the ADE7880 will meter DC. The issue is performance. There are dc offsets from the ADC that vary with temperature and there is no way to compensate for this. when measuring AC the high pass filter removes this dc offset. I do not recommend using the ADE7880 for DC measurement. What sensors are you planning to use to measure current? For DC measurement the ADE9113 with ADE9178 or ADE9113 and a micro controller might be a better option. Possibly the ADEMA124 or ADMA127 with a micro 

    Note the working voltage of the ade9113 you may need the ADE9103 or ADE9102 and separate isolation. 

    Dave

Reply
  • In theory disabling the high pass filter the ADE7880 will meter DC. The issue is performance. There are dc offsets from the ADC that vary with temperature and there is no way to compensate for this. when measuring AC the high pass filter removes this dc offset. I do not recommend using the ADE7880 for DC measurement. What sensors are you planning to use to measure current? For DC measurement the ADE9113 with ADE9178 or ADE9113 and a micro controller might be a better option. Possibly the ADEMA124 or ADMA127 with a micro 

    Note the working voltage of the ade9113 you may need the ADE9103 or ADE9102 and separate isolation. 

    Dave

Children
  • We would like to clarify that our measurement focus is DC only, and we intend to move away from AC measurement in this application.

    We prefer to keep our current schematic if the accuracy and reliability are acceptable after configuration changes; otherwise, we will plan to migrate to the recommended solution.

    We are considering using Hall-effect current sensors (or a DC-capable alternative) for measuring the ~2000 A current at ~470 V. Do you have any evaluation board or reference design based on the ADE9113 (or one of the other recommended devices) that supports high-voltage DC measurement, which we could use as a development reference?

    Additionally, do you have a recommended IC for measuring both AC and DC in a single solution (for future flexibility)?

    We would appreciate any available documentation, board part numbers, or support you can provide for proceeding with a suitable solution.

    Best regards,
    Athul E

  • We are planning to use Hall-effect current sensors (or another DC-capable sensor) to measure approximately 2000 A at 470 V DC. Do you have any evaluation boards, reference designs, or application notes that demonstrate high-voltage DC measurement with your recommended metering ICs that we could use as a development reference?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.