Hello.
Is it possible to monitor normal and reverse power flow using the ADE9000 power monitor?
I think it can be determined from the phase of the current.
Thanks
ADE9000
Production
The ADE9000 is a highly accurate, fully integrated, multiphase energy and power quality monitoring device. Superior analog performance and a digital signal...
Datasheet
ADE9000 on Analog.com
Hello.
Is it possible to monitor normal and reverse power flow using the ADE9000 power monitor?
I think it can be determined from the phase of the current.
Thanks
Hi Osamu,
It is certainly possible to monitor power flowing in both directions with the ADE9000.
The PWATT_ACC and NWATT_ACC registers provide accumulated power in both directions from all 3 phases. The Power Accumulation section of the ADE9000 datasheet has a brief explanation on that functionality. It is also possible to get more detailed information if needed in the application.
Regards,
Jason
Thank you for your reply.
This is for a solar panel project.
I would like you to introduce any devices other than the ADE9000 that have similar functions.
It would be easier to understand if there were items in the parametric research.
Thanks
Osamu
Is this 3ph or DC?
Which additional features are needed?
Regards,
Jason
Hi
It's 3 phase.
I thought it would be nice if additional functions were available when selecting the device.
Thanks