Hello everyone,
I tried making a circuit with the ADE7753 and encountered some issues that damaged my ADE. Initially, I combined the voltage divider circuit and the current measurement CT circuit with the power supply circuit. When I powered on without connecting AGND between the power supply circuit and the ADE circuit, there were no apparent issues. However, when I connected AGND to the ADE circuit, resistors R2, R5, R6, R7, and FB1 in the ADE circuit all burned out along with my ADE. Upon checking, I realized that I used 22pF capacitors (C8 and C9) instead of 100nF, but I don't think that was the cause. I didn't find significant differences in my schematic compared to the proposed design. Can someone help me identify the issue
Thank you!
This is my schematic