I have a problem with a program to connect ADE7753 and Arduino Uno. I made a pcb (photo). I'm using this library: https://github.com/chandrawi/ADE7753/tree/main. When I upload the example code for energy meter it's happens something like this on the photo. I have connected only + 5V to the pcb, without connecting 230 V and current transformer. What am I doing bad? Can somebody help with the code? How I have to calibrate ADE7753?
The code is: