Post Go back to editing

3-phase, 3-wire Delta Connection with ADE7933/ADE7932

Category: Hardware

Hello,

for my final dissertation at university i am trying to design a 3-phase, 3-wire energy meter using ADE7932 and ADE7978. 
I found many helpful documents like the application note AN-1333 and the design files from the EVAL-ADE7978,  but there are questions remaining.



You can see in the figure that the basic structure is clear.I am going to take for the red resistors >1.5M Ohm and for the blue resistors 1k Ohm to measure 400V RMS.

Now both ADE7932 are floating on the specific phase potential. I couldn't find a direct answer if the ADE7932 intern Isolation can handle such big voltages.

Do i have to connect the green dots with the GND_ISO potential of each ADE in addition so the current and voltage measurement have a reference ?



thank you for helping me out.



 

Parents
  • The green dots go to the iso_gnd for the channel talking the measurement. Phase B is reference for the voltage measurements the 1 meg is connected to phase B

    table 7 has the regulatory approvals for working and pk voltage. Check which standards apply to your design. basic or reinforced pollution degree and material group.  

    Dave

Reply
  • The green dots go to the iso_gnd for the channel talking the measurement. Phase B is reference for the voltage measurements the 1 meg is connected to phase B

    table 7 has the regulatory approvals for working and pk voltage. Check which standards apply to your design. basic or reinforced pollution degree and material group.  

    Dave

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.