Post Go back to editing

How do i setup the tdk current transformers with the eval ade9000 shield board?

Category: Hardware

Hi Analog Team,

I've acquired TDK CTs as per the Analog guide.

Please guide me on how to setup the CTs to the evaluation board. Would I just need to put the 3phase 4 current wires through the CT clamps while the CT do not need to be connected to the arduino zero, correct?

Looking forward to your kind reply.

Thank you very much.

Edit Notes

updated
[edited by: Nabil83 at 11:54 PM (GMT -4) on 15 Oct 2023]
Parents Reply
  • This is the recommended input that I shared above. 

    I don't understand this ."And the reason we ran it at max of 80Amps was because of the max Amp value stated for the IC to ensure that it could cope with the load."  you will need to calculate the burden resistor  based on max value, you had indicated 5Amp but tested at 80A

    Dave 

Children
No Data