Post Go back to editing

How do i setup the tdk current transformers with the eval ade9000 shield board?

Category: Hardware

Hi Analog Team,

I've acquired TDK CTs as per the Analog guide.

Please guide me on how to setup the CTs to the evaluation board. Would I just need to put the 3phase 4 current wires through the CT clamps while the CT do not need to be connected to the arduino zero, correct?

Looking forward to your kind reply.

Thank you very much.

Edit Notes

updated
[edited by: Nabil83 at 11:54 PM (GMT -4) on 15 Oct 2023]
Parents Reply
  • Dave,

    Hope youre doing alright. Ive ran tests using the TDK CTs recommended in the technical datasheet, we ran the power source to 80A, however because the CT ratio is 3000:1, at 80A it is barely 0.02 at the IC, so in the Arduino Source Monitor it doesnt even register it at 0.02, it just stays at 0.01. Can you please guide me on improving what I had done? Thanks in advance.

Children