Hi,
I have ADSW-PQ-CLS Power Quality Library integrated with STM32H723ZG in IAR embedded workbench. The project is compiled and running successfully but I have some queries as follows.
1) I am using CLI with following commands.
- setdisplay all off
- setconfig nominalFrequency 50
- setdisplay iharm on
- setdisplay 1012cycles on
- setconfig channels VA
- start 1000
IHARM,1012Cycles,VC,96,6,21260,Y,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00
IHARM,1012Cycles,VC,97,7,21460,Y,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00
IHARM,1012Cycles,VC,98,8,21660,Y,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00
IHARM,1012Cycles,VC,99,9,21860,Y,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00
Here it can be seen there are zero's interharmonics at CLI output and I have generated interharmonics for U1 line using CALMET C300B calibrator and Tester and the interharmonics are verified on oscilloscope.
did I miss something?
2) does the 10/12 cycle count maintain or handled inside APIs? I need a proper Application note to use APIs in a programming model and a flow chart.
With Regards,
Nitin Rawal