Post Go back to editing

ADE9430 ADSW-PQ-CLS Power Quality Library Parameters are not displayed.

Category: Software
Product Number: ADSW-PQ-CLS Power Quality Library
Software Version: Release 1.2.0

Hi,

I have ADSW-PQ-CLS Power Quality Library integrated with STM32H723ZG in IAR embedded workbench. The project is compiled and running successfully but I have some queries as follows.

1) I am using CLI with following commands.

  • setdisplay all off
  • setconfig nominalFrequency 50
  • setdisplay iharm on
  • setdisplay 1012cycles on
  • setconfig channels VA
  • start 1000

 IHARM,1012Cycles,VC,96,6,21260,Y,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00
IHARM,1012Cycles,VC,97,7,21460,Y,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00
IHARM,1012Cycles,VC,98,8,21660,Y,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00
IHARM,1012Cycles,VC,99,9,21860,Y,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00

Here it can be seen there are zero's interharmonics at CLI output and I have generated interharmonics for U1 line using CALMET C300B calibrator and Tester and the interharmonics are verified on oscilloscope. 

did I miss something?

2) does the 10/12 cycle count maintain or handled inside APIs? I need a proper Application note to use APIs in a programming model and a flow chart.

With Regards,

Nitin Rawal 

Parents Reply Children
No Data