Post Go back to editing

ADE1201ACCZ conversion time

Category: Software
Product Number: ADE1201ACCZ

Hi Team,

i need ADE1201ACCZ  ADC Conversion Time for this chip ,

I used this chip in replacement of Si8900 - 2.5 μs conversion time  i have some issue in my logic convertion at the time of 1KHz Signal i need Positive reading only buit as ADC read faster i have both reading positive and 0 , and positive reading with longer delay .

any sugestation on this ?

Regards,

Nikunj

Parents
  • Hi,

    The ADE1201 converts at 100 kHz and the ADE1202 at 50 kHz.

  • Hi Dlath,

    thank you for the update ,

    should i consider 10usec conversation time ?

    at the star it require 150ms for power on reset then 320us for value sampled after that microprocessor can access value over SPI , once it start it require only 10usec to get the updated value right ? 

    it it is correct then i can read 1KHz signal ( high pulse only ) without any delay right ? 

    i have some problem in implementation when i go for read it always detect 0V and after 3-4 sec i get high pulse is there any guide for PWM sensing then please guide me . ( i will try Threshold sensing for batter result  )

    Regards,

    Nikunj

Reply
  • Hi Dlath,

    thank you for the update ,

    should i consider 10usec conversation time ?

    at the star it require 150ms for power on reset then 320us for value sampled after that microprocessor can access value over SPI , once it start it require only 10usec to get the updated value right ? 

    it it is correct then i can read 1KHz signal ( high pulse only ) without any delay right ? 

    i have some problem in implementation when i go for read it always detect 0V and after 3-4 sec i get high pulse is there any guide for PWM sensing then please guide me . ( i will try Threshold sensing for batter result  )

    Regards,

    Nikunj

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.