Post Go back to editing

ADE7858A Phase B failure detection in 3 wire delta system

Product Number: ADE7858A

I have a 3 phase delta configuration  on a ADE7858A meter using 2 CTs, is it possible to detect the lost of phase B between the meter and the load? (the load is a 3 phase motor so it should be a balanced load)

Using a resistive load the current and watts do not seem to change.

The ACCMODE CONSEL is set to 01

Thanks