Post Go back to editing

ADE9078 Energy Readings

Category: Software
Product Number: ADE9078

I have some qusitoin about ADE9078 ,
I had desgin my pcb using ADE9078 and Its work well , I can read Voltage, current ,power, PF and other reading and it seem good

I want to know to Ask about : 

1- I face a problem in reading energy value , 

the energy reading it stat work and accumulating but then it reset to zero when the accumalation reatch to 10.45 each time , I do know the reson

this is the rigister configuration I used 

configured the xGAIN registers,
configured the ACCMODE register with 0x0000 (4-wire wye, 50Hz, Signed active and reactive power/energy accumulation mode),
configured the VLEVEL register with 0x00117514 as suggested in page 56 of User Manual,
configured the CONFIG0 register with 0x00000000 as we use a 1000:1 Current Transformer
Additionally, as we need to read the energy register with reset, we followed what is stated at page 43 of User Manual:

configured the EGY_TIME register with 0xF9F

1,configured the EP_CFG register with 0xE001(RD_RST_EN=0, EGY_LD_ACCUM=0, EGY_TMR_MODE=0, EGY_PWR_EN=1, NOLOAD_TMR=111,PWR_SIGN_SEL=0)

void ADE9000Class::ReadActiveEnergyValue(ActiveEnergyRegVlaue *Data)
{
	int32_t temp_lowpacke; 
	int32_t temp_highpacket;  
	
	temp_lowpacke   = int32_t (SPI_Read_32(ADDR_AWATTHR_LO))>>19; 
    temp_highpacket = int32_t (SPI_Read_32(ADDR_AWATTHR_HI)) ; 

	Data->totalActiveEnergy_A =  (temp_highpacket << 13)|temp_lowpacke ;
	

}

this is code and Library which I used currently 

drive.google.com/.../view

2-I have a problem in Frequency value it's 51.4Hz and actual value is 50Hz 
it would be calibration issue or I need make some Calculatotion??
I have Some doubt becase I am use different Crystals value I use 12MHz , but the recomended 12.288MHz
may this changing make the freq. reading wrong ?

3- can I read the line to line Voltage in ADE9078  ?
an example can I read Vab =480V ?
If I use the same wire configuration wye ,
what shoud be wire congiguration to have both reading line ot line voltage(Vab) and line to nutral voltage (Va)

4- Can I  Read the Harmonics value when using ADE9078 ?