Post Go back to editing

asking about ADE7763 Vrms and Irms register value

Category: Datasheet/Specs
Product Number: ADE7763

hi everyone. im new at this forum

i want to ask about ADE7763 Vrms and Irms register value.

as i known when i read datasheet, the Maximum value between V1p-V1n and V2p-V2n is 0.5V peak, the maximum rms value can reach is 1868467d (0x1C82B3) in the IRMS register , and 1561400 (0x17D338) in the VRMS register  

so to test it out, i use Analog Discovery 2 to generate the waveform to V1p-V1n, V2p-V2n pins. below is the result.

both V1p-V1n, V2p-V2n input = 100mv --> Vrms =329827        Irms =387625

both V1p-V1n, V2p-V2n input = 200mv --> Vrms =659837        Irms =775532

both V1p-V1n, V2p-V2n input = 300mv --> Vrms =989431        Irms =1163034

both V1p-V1n, V2p-V2n input = 400mv --> Vrms =1319889      Irms =1550859

both V1p-V1n, V2p-V2n input = 500mv --> Vrms =1649628      Irms =1938418

both V1p-V1n, V2p-V2n input = 600mv --> Vrms =1978903      Irms =2325707

both V1p-V1n, V2p-V2n input = 700mv --> Vrms =2308025      Irms =2713455

...

the more input voltage increase, the more Vrms, Irms increase. there are no limit here

Can someone points out where I'm going wrong?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.