Hi,
ADE9153A - How can I program a pulse output that generates exact 1600 pulses at 1KWh active power ?
Can the number of pulses be calculated ?
ADE9153A
Recommended for New Designs
The ADE9153A is a highly accurate, single-phase, energy metering
IC with autocalibration. The mSure® autocalibration feature allows a meter to automatically...
Datasheet
ADE9153A on Analog.com
Hi,
ADE9153A - How can I program a pulse output that generates exact 1600 pulses at 1KWh active power ?
Can the number of pulses be calculated ?
Hi, you need to go through a calibration procedure in order to set the impulses/kWh of the CF output.
First off you can use either the CF1 or CF2 pins to generate this pulse.
Then you have the calculate the CFxDEN value that gets you the impulses/kWh you are looking for with the following equations:
xTHR should be left at the default of 0x00100000
If:
Then CFxDEN = 0xFFF
TARGET_WCC can be calculated using equation 4 on page 6 of AN-1571 (Rev. 0) (analog.com)
Hi, you need to go through a calibration procedure in order to set the impulses/kWh of the CF output.
First off you can use either the CF1 or CF2 pins to generate this pulse.
Then you have the calculate the CFxDEN value that gets you the impulses/kWh you are looking for with the following equations:
xTHR should be left at the default of 0x00100000
If:
Then CFxDEN = 0xFFF
TARGET_WCC can be calculated using equation 4 on page 6 of AN-1571 (Rev. 0) (analog.com)