Post Go back to editing

ADE9000 xWATTHR register not reset

Category: Hardware
Product Number: ADE9000

Hello everyone.

We are building an energy meter with the ADE9000 and came across an issue with the xWATTHR register.

The ADE is set up to reset the register after every read, but every other hour we see a value twice the expected one.

This lets us think, that the register was not reset after the last read.

We are already reading the register twice to force a reset and decrease the probability of a skipped reset.

Is this an know issue?

Is there another way to ensure the register reset?

Thanks in advance!

Parents
  • I'm seeing the same. Applying a constant test signal, will return a value that is twice the expected value. This happens completely randomly but with what looks like a ~1:50000 chance. It totally feels like a race condition or read-modify-write bug in the ADE9000 firmware. Would be great if one of the devs could have a look at the code.

  • I would suggest you use line cycle or sample based accumulation and read on irq or using the status register. 

    What is the benefit of read with reset in your application as apposed to reading at a fixed period  based on line cycle or sample based? 

    Dave

  • In my case the reading of the registers is synchronized to the wall clock down to a resolution of 100ms. It would maybe be possible to find a solution that does not need reading the WATTHR register with reset, but it would complicate our firmware and make it less accurate (in relation to the measurement timestamps). What I would probably do, if this is indeed a confirmed bug in the ADE9000.

    If it's a bug, it should be documented at least, if not fixed in the ROM mask.

  • What may be helpful to you is sync your read to dready 

    wait for time clock period then 

    wait for dready using  irq or status

    read registers

    see if this helps.

    As far as debugging this how often are you reading the registers? You mention 100 ms above is that the fastest you read. 

    Dave

  • So far the only time I have had an issue is if the micro is servicing an IRQ. Can you add a time stamp when you read the energy registers?

    I did my test without any inputs and only 1 channel for my test

    epconfig = 0x21

    1 write xIGAIN and xVGAIN registers to 0xF8000000 this will set gain to 0 and force datapath to 0 

    ADE_SPI_WRITE(ADDR_AIGAIN,0xF8000000,0x4);

    2 write Xwattos to any value. This is just  number to accumulate at the sample rate. I used 0x228BA2

     ADE_SPI_WRITE(ADDR_AWATTOS,0x228BA2,0x4);

    in my loop 

    void loop(void){
    if (millis() - period_ms > 100)
    {
    period_ms = millis();
    energy = ADE_SPI_READ(ADDR_AWATTHR_HI,0x04);
    if(energy < 212000 | energy > 283000)
    Serial.println(energy);
    }

    These are the values I read at 100ms and used this data to set if(energy < 212000 | energy > 283000)  

    If I get any failures I will post later

    212247
    212247
    212248
    282996
    212247
    212247
    212247
    212248
    212247
    282996
    212247
    212247
    212248
    212247
    212247
    212247
    282996
    212248
    212247
    212247
    212247
    212247
    282997
    212247
    212247
    212247
    212247
    212248
    282996
    212247
    212247
    212247
    212248
    212247
    212247
    282996
    212247
    212248
    212247
    212247
    212247
    282996
    212248
Reply
  • So far the only time I have had an issue is if the micro is servicing an IRQ. Can you add a time stamp when you read the energy registers?

    I did my test without any inputs and only 1 channel for my test

    epconfig = 0x21

    1 write xIGAIN and xVGAIN registers to 0xF8000000 this will set gain to 0 and force datapath to 0 

    ADE_SPI_WRITE(ADDR_AIGAIN,0xF8000000,0x4);

    2 write Xwattos to any value. This is just  number to accumulate at the sample rate. I used 0x228BA2

     ADE_SPI_WRITE(ADDR_AWATTOS,0x228BA2,0x4);

    in my loop 

    void loop(void){
    if (millis() - period_ms > 100)
    {
    period_ms = millis();
    energy = ADE_SPI_READ(ADDR_AWATTHR_HI,0x04);
    if(energy < 212000 | energy > 283000)
    Serial.println(energy);
    }

    These are the values I read at 100ms and used this data to set if(energy < 212000 | energy > 283000)  

    If I get any failures I will post later

    212247
    212247
    212248
    282996
    212247
    212247
    212247
    212248
    212247
    282996
    212247
    212247
    212248
    212247
    212247
    212247
    282996
    212248
    212247
    212247
    212247
    212247
    282997
    212247
    212247
    212247
    212247
    212248
    282996
    212247
    212247
    212247
    212248
    212247
    212247
    282996
    212247
    212248
    212247
    212247
    212247
    282996
    212248
Children