Post Go back to editing

ADE7880 - Rogowski coil not working

Hello,

I designed a circuit for energy monitoring using CT and Rogowski , this is done by  closing and opening appropriate jumpers across burden resistor, fig shown below

I tested the circuit for Rogowski with all jumpers open,  and on the software side I turned ON integrator by 

// SPIWrite2Bytes(DICOEFF,0xFF8000);
SPIWrite2Bytes(CONFIG,0x0001);  // integrator on

But the output is not correct

IC is not changing .

But in the case of CT, it's working i closed jumpers for CT as mentioned in the ADE7880_userguide.

what is the issue with Rogowski, 
please Help.

Edit Notes


[edited by: vivekpkd at 11:29 AM (GMT -4) on 21 Mar 2022]
Parents
  • You need to remove/ disconnect the burden resistor. The Rogowski coil can't drive a load that low. 

    Dave

  • Yes, i didnt soldered burden resister, i have seen similar questions about that. 

  • Are you using the same calibration for ct and Rogowski coil?   You will need  separate calibration for each sensor. 

    The amps/volt  for each sensor are different. 

    Dave

  • calibration needs to be done after all the basic configurations are made for each sensor such as enabling or disabling the integrator

  • Hi,   from the debugging, I found that the issue is before the calibration, ie the Current value IC is always "8388607" (integrator ON) with and without connecting Rogowski cable, 

    my code for Reg config is 

    void ADE7880_REG_Config(void)
    {
        SPIWrite2Bytes(COMPMODE,0x00FF);
    
    
       // SPIWrite4Bytes(VLEVEL,0x00B3DA8D);
    
        SPIWrite2Bytes(APHCAL,0x032F);//powrfactor calliberation32f
        SPIWrite2Bytes(BPHCAL,0x032F);
        SPIWrite2Bytes(CPHCAL,0x032F);
    
    	SPIWrite2Bytes(Gain,0x0000);	//0000		  //config the  Gain of the PGA , which is before the ADC of ADE7878
    	SPIWrite2Bytes(CONFIG,0x0000);
    	  SPIWrite2Bytes(DICOEFF,0xFF8000);
    	SPIWrite2Bytes(CONFIG,0x0001);			  // integrator on
    
    	SPIWrite1Byte(CONFIG3,0x00);			  //enabled high-pass filters
    
    	SPIWrite4Bytes(AIGAIN,0x00000000);		  //calibration
    	SPIWrite4Bytes(AVGAIN,0x00000000);
    	SPIWrite4Bytes(BIGAIN,0x00000000);
    	SPIWrite4Bytes(BVGAIN,0x00000000);
    	SPIWrite4Bytes(CIGAIN,0x00000000);
    	SPIWrite4Bytes(CVGAIN,0x00000000);
    	SPIWrite4Bytes(NIGAIN,0x00000000);
    
     	SPIWrite4Bytes(AIRMSOS,0x00000000);
    	SPIWrite4Bytes(AVRMSOS,0x00000000);
    	SPIWrite4Bytes(BIRMSOS,0x00000000);
    	SPIWrite4Bytes(BVRMSOS,0x00000000);
    	SPIWrite4Bytes(CIRMSOS,0x00000000);
    	SPIWrite4Bytes(CVRMSOS,0x00000000);//F06E
    	SPIWrite4Bytes(NIRMSOS,0x00000000);
    
     	SPIWrite4Bytes(APGAIN,0x00000000);
    	SPIWrite4Bytes(AWATTOS,0x00000000);
    	SPIWrite4Bytes(BPGAIN,0x00000000);
    	SPIWrite4Bytes(BWATTOS,0x00000000);
    	SPIWrite4Bytes(CPGAIN,0x00000000);
    	SPIWrite4Bytes(CWATTOS,0x00000000);
    
    	SPIWrite2Bytes(APHCAL,0x0000);
    	SPIWrite2Bytes(BPHCAL,0x0000);
    	SPIWrite2Bytes(CPHCAL,0x0000);
    
    	SPIWrite2Bytes(CF1DEN,0x00A7);	  		  //configure the ENERGY-TO-FREQUENCY
    	SPIWrite2Bytes(CF2DEN,0x00A7);
    	SPIWrite2Bytes(CF3DEN,0x00A7);
    	SPIWrite2Bytes(CFMODE,0x0E88);
                                        //CF1-total active power, disable; CF2-total reactvie power, disable; CF3- fundamental avtive power, disable
        //SPIWrite4Bytes(HCONFIG,0x000002A2);
         SPIWrite2Bytes(HCONFIG, 0x0000);
    
    	SPIWrite2Bytes(ACCMODE,0x0000);
    
    
    //	SPIWrite2Bytes(COMPMODE,0x00FF);
    
    	SPIWrite1Byte(MMODE,0x00);
    
    	SPIWrite1Byte(HX_reg,0x03);
    	SPIWrite1Byte(HY_reg,0x03);
    	SPIWrite1Byte(HZ_reg,0x03);
    
    
    	SPIWrite4Bytes(WTHR,0x007BBE61);			  //PMAX = 33,516,139	  0.001WH/LSB	 //page 47 datasheet Rev. E
    //	SPIWrite4Bytes(WTHR1,0x00000017);
    	SPIWrite4Bytes(VATHR,0x007BBE61);		  //PMAX = 33,516,139
    //	SPIWrite4Bytes(VATHR1,0x00000017);
    	SPIWrite4Bytes(VARTHR,0x007BBE61);		  //PMAX = 33,516,139
    //	SPIWrite4Bytes(VARTHR1,0x00000017);
    //    SPIWrite4Bytes(VLEVEL,0x007BBE61);
       //SPIWrite4Bytes(VLEVEL,0x005DD633);
          SPIWrite4Bytes(VLEVEL,0x000C1ECC);
        //0xB3DA8D
    
    	SPIWrite1Byte(LCYCMODE,0x08);				  //phase B is selected for zero cross
    	SPIWrite2Bytes(LINECYC,0x0064);
    
    	SPIWrite4Bytes(MASK0,0x00000020);			  //line cycle interrupt enable
    	SPIWrite4Bytes(MASK1,0x00000000);
    // for flushing the data  write additional 2 times
    	SPIWrite4Bytes(MASK1,0x00000000);
    	SPIWrite4Bytes(MASK1,0x00000000);
    
    }

  • Please verify input ckt is configured like this

    I don't see the run bit being set in the code above. you could be doing in somewhere else just verifying the run bit is set. 

    What is the state of the psm0 and 1 pins. 

    If the Rogowski is not connected or is connected but not correctly (see ckt above) there may be to much noise. 

    you are using a PGA gain of 1 for the current channel is this correct for your Rogowski coil? 

    Dave

Reply
  • Please verify input ckt is configured like this

    I don't see the run bit being set in the code above. you could be doing in somewhere else just verifying the run bit is set. 

    What is the state of the psm0 and 1 pins. 

    If the Rogowski is not connected or is connected but not correctly (see ckt above) there may be to much noise. 

    you are using a PGA gain of 1 for the current channel is this correct for your Rogowski coil? 

    Dave

Children