ADE9153 calibration source specifications

Dear Sir,

There are no specifications for the 3 calibration sources on the ADE9153 datasheet for IAMS, IBMS, and VAMS.  For each source what is the frequency, duty cycle, current and voltage compliance if a current source, along with the high and low current level and if a voltage source the high and low level output voltages and the maximum current that can be drawn.

Cheers

DrBill

  • 0
    •  Analog Employees 
    on Oct 29, 2021 5:15 PM

    Hi DrBill,

    All the specifications for the mSure feature are given in the data sheet, we do not provide specifications beyond that.

    What is it that you are trying to understand? If you have a specific issue then I can help you work through it.

    If you are looking for the largest shunt value which can be used on the IAMS channel, we don't recommend going any larger than a 23 mOhm shunt. If the sensor is too large for any channel, it will trigger the MS_OVERFLOW bit to let you know that the signal is over-ranging.