Post Go back to editing

Multiplexed current input to ADE7880

Hi,

Is it possible to connect more than 3 current inputs to ADE7880 via multiplexing.

For eg; we are collecting 16 inputs from CT.'s and multiplexed those inputs and sending to adc pins of microprocessor.

Like that is it possible to connect this multiplexed input to channel A,B,C of ADE7880?

Parents
  • Anything is possible but at a cost. 

    When switching multiple ct's to a single adc input you have to wait for the data to settle. The sinc , lpf high-pass and lpf2 filters need to settle and this can take seconds in total time before the output meets datasheet specs. 

    You will also need to calibrate each CT and change any gain/phase correction for each CT. 

    I think This is an over complicated task. 

    Why would you not use multiple ade7880. This seem to be a better option. 

    Dave 

  • Hi,

    If I use five ADE chip, it will have five  SPI out from ADE to processor. So how can we connect this five ADE chip to a single processor.

    What is the difference between ADE9000 and ADE7880?

    For ADE9000, i have doubt of can we connect Rogowski & CT to the same circuit (or  doing in software) , for ADE7880 we have two different circuits for Rogowski & CT

    if we go for multiple Ade chips, we need to have 5 Ade chips to connect 15 lines (R, Y, B Phase) that is 5 equipment's & 5 Neutral lines. For power signature analysis, which one is better ADE9000 or ADE7880? What is the major difference between these two ADE chip.

Reply
  • Hi,

    If I use five ADE chip, it will have five  SPI out from ADE to processor. So how can we connect this five ADE chip to a single processor.

    What is the difference between ADE9000 and ADE7880?

    For ADE9000, i have doubt of can we connect Rogowski & CT to the same circuit (or  doing in software) , for ADE7880 we have two different circuits for Rogowski & CT

    if we go for multiple Ade chips, we need to have 5 Ade chips to connect 15 lines (R, Y, B Phase) that is 5 equipment's & 5 Neutral lines. For power signature analysis, which one is better ADE9000 or ADE7880? What is the major difference between these two ADE chip.

Children
No Data