Post Go back to editing

ADE7880 single phase three wire (AB line connect to meter actually)

Hello

        Customer would like use ADE7880 for single-phase three wire (But Phase A & Phase B line connect to meter actually). The power environment is PhaseA and PhaseB (VAB=220V). But neutral wire will not input to meter (ADE7880). In other words, Only phase A and Phase B connect to ADE7880 (Fig. 1). Has any doc or reference schematics of ADE7880 for this connection? How to connect Phase A and Phase B to ADE7880?   

        Another question for Fig 2. the register of ADE7880 should have IA and IB ? But how to calculate VAB and IAB value or get these information by above meter setup? it is a little urgent and looking forward to receiving a reply. Thank you.  

Fig,1 

Fig 2. 

  

BR

Patrick



Modify words
[edited by: patrickchen@morrihan.com at 3:57 AM (GMT -4) on 12 May 2021]
Parents
  • Hi Patrick,

    Does this answer your question? Am I understanding you question correctly?

    220 currents IABRMS = IARMS +IBRMS   no it does not. 

         Only common currents are 220    IABRMS=((IARMS+IBRMS) - (ABS(IARMS-IBRMS)))/2

    110 currents IBRMS=IBRMS - IABRMS 

    110 currents IARMS=IARMS - IABRMS 

    XLSX

  • Hello

           Thanks for reply. Below is schematics and question. Could you help provide comments?  It is a little urgent and look forward to receive reply. Thank you. Thank you. 

    1. IC (channel C – ICN ICP) does not use
    2. IN (Channel N – INN INP) does not use
    3. VAB à what is the mean ? what define pin? VAP?
    4. The our schematic is summarized below image

            

    BR

    Patrick

Reply
  • Hello

           Thanks for reply. Below is schematics and question. Could you help provide comments?  It is a little urgent and look forward to receive reply. Thank you. Thank you. 

    1. IC (channel C – ICN ICP) does not use
    2. IN (Channel N – INN INP) does not use
    3. VAB à what is the mean ? what define pin? VAP?
    4. The our schematic is summarized below image

            

    BR

    Patrick

Children