Post Go back to editing

ADE9078 reading Issue

Hi,

We are working on energy meter IC ADE9078. Our micro controller is used to communicate with three energy meter IC through three SPI Isolator ADUM3150.

While reading value of VLEVEL status from  three energy meter, it showing always zero. It's not reading proper also.

Note: we have put tri-state buffer on energy meter side and SPI Isolator.

In ADUM3150 datasheet , it mention don't need of tri-state buffer while using this isolator. But if we removed two SPI isolator, one energy meter is working fine.

Please give suggest us to get out of this problem.

Regards,

Poovai.L

  • Hi Poovai, 

    The ADuM3150's MI channel is always driven. If there are multiple ADuM3150 devices on the SPI bus, the MI channel will need a tri-state buffer installed to prevent the different outputs attached to the same MISO signal trace from being in contention. 

    Regards,

    Jason 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.