Post Go back to editing

Energy Metering device based on ADE7755 with MCU

Hello, I am completely new in this. 

I'm trying to do college project. 

I've done this schematic based on ADE7755 datasheet and AN-559 application node. My knowledge about this is not great. Could this schematic work?

For power supply I'm using two 9V batteries with LM7805 to reduce it to 5V. They are used separately for MCU and ADE7755.

I chose ADE7755 because its one of very few available to buy in my country (most are to buy in bulk).

I saw in datasheets grounded phase wire. How to do that properly? Cut a little of isolation from the wire and just ground it?

Also, for voltage transformer I'm using BV 202 0158 HAHN with double secondary to reduce voltage from 230V→2x 9V. I'm conversing it to center-tapped transformer by connecting middle pins and grounded it. CT is  1000:1 40A. With burden resistors 2x 2.4ohms grounded in the middle.

In ADE datasheet I saw two outputs from optocoupler, from emitter and collector. How does it work? Can I connect only one output to the MCU to count the pulses? 

BTW I am sorry for my English, it's not my first language ;)

Full schematic with MCU

  • Thank you. I have another thing that I don't understand. I'm using PT and CT in single-phase metering, do I still need to ground phase line or is it only when using shunts? 

  • If you are using a pt and a ct. Neutral does not need to be connected to your analog ground.  All your pt and ct should be tie to ground some how like you did in your schematic above. You voltage divider goes to analog ground and your burden is center tapped to analog ground. 

    Dave 

  • Hi  
    Were you able to get this working? If yes, I would like to ask you some follow up question. Any positive feedback from you would be greatly appreciated.
    Thank you in advance.

  • Hi  
    Please, I am trying to do something similar to this but I want to be able to read a minimum of 4 currents channels that is from 4 different 4 A.C loads. Please, any ideas on how I could get started on this?
    I am currently a newbie on this sphere but I can pick up very quickly if I put my mind to it all.

    Your response would be greatly appreciated. Thank you.

  • Do you need power or just Current RMS and Voltage RMS. or power also. 

    Look at the ADE7816  6 current channels and 1 voltage channel. 

    Dave

  • Thank you  
    I have checked out the ADE7816 Energy IC. And I can see it can do what I want to do. Which is to be able to measure both power and energy (both real and apparent forms of them) on various A.C loads on a single phase line. But like I initially mentioned, I am currently new in power electronics. 
    And I couldn't find the application note to show me how to show a well detailed schematic diagram for the IC itself. 
    What I want to do is to be able to use any of the such IC or some other one like ADE7878 or ADE7953. to measure the energy using an MCU like Atmega328P or any other Arduino based board. Or even the ESP32 board using either I2C or SPI communication protocol.

    I would have used a PZEM module but I would be looking at huge cost as I increment the number of modules, and also, the problem of communication with the MCU. But most importantly, I am trying to reduce cost. 

    If I could get an Energy IC that could be cascaded as the demand of the load increases and also have a head start on the Arduino programming. I could be forever grateful.

    Regards,
    AncII

  • ADE7878 and ADE7816 are pin for pin compatible. The ADE7816 have been modified to measure 1v and 6 I using CTs

    Please post question in one place. 

    Here are some arduino code examples to help get comms going using SPI. 

    Dave

    1222.ade7953_bluepill_spi_cal_5_17p5_23.TXT

    // eval board notes for use with bluepill adapter board
    // note jumper pin15 and pin14 together on p13 to hold micro in reset. the loop code in micro is not correct for cf2 and cf3 and tried to pull up the pins. 
    // use external vdd from blue pill P1 connector
    // jp 72,73,74 need solder ball to connect external pins on p17 connocts spi pins to external p17. short pas closer to p17 
    // I shorted 12and 3 on j75 j76 j77 to get cf1 2 and 3 to external connector p17
    
    #include <SPI.h>
    #include "ADE7878_REG.h"
    
    void ADE7878_SPI_WRITE(uint16_t Address , uint32_t Data , uint8_t Number_of_bytes);
    uint32_t ADE7878_SPI_READ (uint16_t Address, uint8_t Number_of_bytes);
    void READ_RMS_ENERGIES_PRINT();
    void ADE7878_reg_config();
    void READ_RMS_AVERAGE_PRINT();
    
    //outputs
    #define PM_0 PB15
    #define PM_1 PA8
    #define RESET_B PB3
    #define SSB_A PA4 
    #define SSB_B PB5 
    #define SSB_C PB4 
    #define SCLK PA5
    
    //inputs
    #define CF1 PB6
    #define CF2 PB7
    #define CF3 PC14
    #define IRQ0 PB14
    #define IRQ1 PB13
    #define DREADY PB12
    
    
    //SPI_1 Chip Select pin is PA4. You can change it to the STM32 pin you want.
    //LED1=PC_13  SERIAL_TX=PA_2  I2C_SCL=PB_8  SPI_MOSI=PA_7  PWM_OUT=PB_3
    //            SERIAL_RX=PA_3  I2C_SDA=PB_9  SPI_MISO=PA_6
    //                                          SPI_SCK =PA_5
    
    // bluepill      ADE7878/7880/7816
    //PA4  > SSB_A   >> SSB
    //PB5  > SSB_B
    //PB4  > SSB_C
    
    //PA5  > sclk    >> SCLK
    //PA6  > miso    >> MISO
    //PA7  > mosi    >> MOSI
    
    //PA8  > PM1     >> PM1 
    //PB15 > PM0     >> PM0
    //PB14 > IRQ0    >> IRQ0
    //PB13 > IRQ1    >> IRQ1
    
    //PB9  > sda
    //PB8  > scl
    
    //PB3  > RSTB    >>RESETB
    //PB12 > DREADY  
    
    //PB6  > CF1     >> CF1
    //PB7  > CF2     >> CF2
    //PC14 > CF3     >> CF3
    
    byte data;
    
    int CF1_COUNT = 0;
    int CF2_COUNT = 0;
    int CF3_COUNT = 0;
    byte IRQ_STATUS = 0;
    byte DREADY_COUNT = 0;
    int last_millis = 0;
    int32_t temp;
    float cf_freq = 0;
    uint32_t last_cf_edge;
    
    double IRMS_LSB = 0;
    double VRMS_LSB = 0;
    double WATT_LSB = 0;
    double WH_LSB = 0;
    
    void setup() {
      // put your setup code here, to run once:
      Serial.begin(115200);
      while(!Serial); // wait for serial poert to be open
      
      SPI.begin(); //Initialize the SPI_1 port.
      SPI.setBitOrder(MSBFIRST); // Set the SPI_1 bit order
      SPI.setDataMode(SPI_MODE3); //Set the SPI_2 data mode 0
      SPI.setClockDivider(SPI_CLOCK_DIV32);      // Slow speed (72 / 16 = 4.5 MHz SPI_1 speed)
      
      pinMode(SSB_A, OUTPUT);
      pinMode(RESET_B, OUTPUT);
      pinMode(PM_0, OUTPUT);
      pinMode(PM_1, OUTPUT);
      
    
      digitalWrite(SSB_A, HIGH);
      digitalWrite(RESET_B, HIGH);
    
      digitalWrite(PM_0, HIGH);
      digitalWrite(PM_1, LOW);
    
      digitalWrite(RESET_B, LOW);
      delay(10);
      digitalWrite(RESET_B, HIGH);
    
      pinMode(CF1, INPUT);
      pinMode(CF2, INPUT);
      pinMode(CF3, INPUT);
      pinMode(IRQ0, INPUT);
      pinMode(IRQ1, INPUT);
      pinMode(DREADY, INPUT);
    
    
      //reset part
    
      delay (2000);                 // not recommended use reset done
      //while(digitalRead(IRQ1));   // wait for reset done recommended
    
    
      //set spi port TOGGLE SSB 3 TIMES
      digitalWrite(SSB_A, LOW);
      delay(1);
      digitalWrite(SSB_A, HIGH);
      delay(1);
      digitalWrite(SSB_A, LOW);
      delay(1);
      digitalWrite(SSB_A, HIGH);
      delay(1);
      digitalWrite(SSB_A, LOW);
      delay(1);
      digitalWrite(SSB_A, HIGH);
    
      
      delay(1000);
      
      //ADE7878_SPI_WRITE(STATUS0,ADE7878_SPI_READ(STATUS0, 4),4);   //clr IRQ
      //ADE7878_SPI_WRITE(STATUS1,ADE7878_SPI_READ(STATUS1, 4),4);   //clr IRQ
      //ADE7878_CF_TEST();
      //while(1);
      ADE7878_reg_config();
      //attachInterrupt(digitalPinToInterrupt(DREADY),dready_irq,FALLING); // response about 5.2us
       attachInterrupt(digitalPinToInterrupt(CF1),CF1_irq,FALLING); // response about 5.2us
       attachInterrupt(digitalPinToInterrupt(CF2),CF2_irq,FALLING); // response about 5.2us
       attachInterrupt(digitalPinToInterrupt(CF3),CF3_irq,FALLING); // response about 5.2us
      //attachInterrupt(digitalPinToInterrupt(IRQ0),IRQ0_irq,FALLING); // response about 5.2us
      //attachInterrupt(digitalPinToInterrupt(IRQ1),IRQ1_irq,FALLING); // response about 5.2us
       
    }
    
    
    void dready_irq(){
     DREADY_COUNT++;
    }
    
    void CF1_irq(){
      CF1_COUNT++;
      cf_freq = 1 / ((micros() - last_cf_edge) / 1000000.00);
      last_cf_edge = micros();
    }
    
    void CF2_irq(){
     CF2_COUNT++;
    }
    
    void CF3_irq(){
     CF3_COUNT++;
    }
    
    void IRQ0_irq(){
     ADE7878_SPI_WRITE(STATUS0,ADE7878_SPI_READ(STATUS0, 4),4);   // read and clear irq
    }
    
    void IRQ1_irq(){
     ADE7878_SPI_WRITE(STATUS1,ADE7878_SPI_READ(STATUS1, 4),4);  // read and clear irq
     
    }
    
    
    
    void loop() {
         calibrate_ade7878();
       
    }
    
    
    
    void calibrate_ade7878() {
    
      delay(10000); //wait for RMS to settle
    
      // enter values
      uint16_t V_TEST = 220;//volts RMS
      uint16_t I_TEST = 10;//Amps RMS
      double Power_factor = 1;
      int meter_constant = 1000;  //1000 imp/Kwh for cf output rate
      int Line_Freq = 50;
      int accumulation_time = 3; //sec
    
    
      double R1 = 1000000; //big resistor or sum of upper resisters
      double R2 = 1000; //small resistor
    
      double CT_Ratio = 2000; // to 1
      double burden = 2.5*2; // 2 resisters differential burdens or 1 single burden resistor for single ended.
      
      //constants
    #define  PMAX 33516139
    #define  Sample_Rate 8000
    #define  WTHR_Value 33516139
    #define  V_PGA  1
    #define  I_PGA  1
    #define  I_channel_ADC_FS  (.3535 / I_PGA)
    #define  V_channel_ADC_FS  (.3535 / V_PGA)
    #define  RMS_FS_Codes 4191910 //50hz  
    //#define  RMS_FS_Codes 3493258 //60hz  
    
    
      //calculated
      double Percent_FS_Voltage = (((R2 / (R1 + R2)) * V_TEST) / V_channel_ADC_FS);
      double Percent_FS_Current = ((I_TEST / CT_Ratio) * burden ) / I_channel_ADC_FS;
      double V_Fullscale = V_TEST / Percent_FS_Voltage;
      double I_Fullscale = I_TEST / Percent_FS_Current;
      double Expected_CF_Freq = (meter_constant / 1000 * V_TEST * I_TEST * Power_factor) / 3600;
      //double IRMS_LSB = 0;
      //double VRMS_LSB = 0;
      //double WATT_LSB = 0;
      //double KWH_LSB = 0;
      
      
      uint16_t CFDEN_CAL_VALUE = (uint16_t)(((33516139 / WTHR_Value) * 8000 * Power_factor * Percent_FS_Voltage * Percent_FS_Current) / Expected_CF_Freq);
      int32_t AIGAIN_CAL_VALUE = (int32_t)((((RMS_FS_Codes * Percent_FS_Current) / (double)ADE7878_SPI_READ(AIRMS, 4)) - 1) * 8388608); // 2^23 = 8388608
      int32_t AVGAIN_CAL_VALUE = (int32_t)((((RMS_FS_Codes * Percent_FS_Voltage) / (double)ADE7878_SPI_READ(AVRMS, 4)) - 1) * 8388608); // 2^23 = 8388608
    
      int32_t BIGAIN_CAL_VALUE = (int32_t)((((RMS_FS_Codes * Percent_FS_Current) / (double)ADE7878_SPI_READ(BIRMS, 4)) - 1) * 8388608); // 2^23 = 8388608
      int32_t BVGAIN_CAL_VALUE = (int32_t)((((RMS_FS_Codes * Percent_FS_Voltage) / (double)ADE7878_SPI_READ(BVRMS, 4)) - 1) * 8388608); // 2^23 = 8388608
    
      int32_t CIGAIN_CAL_VALUE = (int32_t)((((RMS_FS_Codes * Percent_FS_Current) / (double)ADE7878_SPI_READ(CIRMS, 4)) - 1) * 8388608); // 2^23 = 8388608
      int32_t CVGAIN_CAL_VALUE = (int32_t)((((RMS_FS_Codes * Percent_FS_Voltage) / (double)ADE7878_SPI_READ(CVRMS, 4)) - 1) * 8388608); // 2^23 = 8388608
    
    
      Serial.println("");
      Serial.print("  V_TEST Used For Calibration = "); Serial.println(V_TEST);
      Serial.print("  I_TEST Used For Calibration = "); Serial.println(I_TEST);
      Serial.print("  Power_factor Used For Calibration = "); Serial.println(Power_factor);
      Serial.print("  Line_Freq Used For Calibration = "); Serial.println(Line_Freq);
      Serial.print("  Accumulation Time Used For Calibration = "); Serial.println(accumulation_time);
      Serial.println("");
    
      Serial.print("  Vlevel Calculated Register Value = "); Serial.println((uint32_t)((V_Fullscale / V_TEST) * 4000000), HEX);
      Serial.println("");
    
      ADE7878_SPI_WRITE(VLEVEL, (uint32_t)((V_Fullscale / V_TEST) * 491520), 4);
      
      Serial.print("  V_TEST = "); Serial.print(Percent_FS_Voltage * 100, 2); Serial.print("% Fullscale"); Serial.print(" = "); Serial.print(V_channel_ADC_FS * Percent_FS_Voltage,4);Serial.print(" VRMS at ADC input and ");Serial.print(V_Fullscale, 2); Serial.println(" VRMS Fullscale");
      Serial.print("  I_TEST = "); Serial.print(Percent_FS_Current * 100, 2); Serial.print("% Fullscale"); Serial.print(" = "); Serial.print(I_channel_ADC_FS * Percent_FS_Current,4);Serial.print(" VRMS at ADC input and ");Serial.print(I_Fullscale, 2); Serial.println(" IRMS Fullscale");
    
      
    
      Serial.println("");
      Serial.print("  Expected_CF_Freq = "); Serial.println(Expected_CF_Freq, 6);
      Serial.print("  CFDEN_CAL_VALUE = "); Serial.println(CFDEN_CAL_VALUE);
      Serial.println("");
    
      ADE7878_SPI_WRITE(CF1DEN, CFDEN_CAL_VALUE, 2);
      ADE7878_SPI_WRITE(CF2DEN, CFDEN_CAL_VALUE, 2);
      ADE7878_SPI_WRITE(CF3DEN, CFDEN_CAL_VALUE, 2);
      
      Serial.print("  AIRMS Expected = "); Serial.println(Percent_FS_Current * RMS_FS_Codes ,0);
      Serial.print("  AVRMS Expected = "); Serial.println(Percent_FS_Voltage * RMS_FS_Codes ,0);
      Serial.print("  AIRMS RAW = "); Serial.println(ADE7878_SPI_READ(AIRMS, 4), DEC);
      Serial.print("  AVRMS RAW = "); Serial.println(ADE7878_SPI_READ(AVRMS, 4), DEC);
      Serial.println("");
      Serial.print("  AIGAIN_CAL_VALUE "); Serial.println(AIGAIN_CAL_VALUE);
      Serial.print("  AVGAIN_CAL_VALUE "); Serial.println(AVGAIN_CAL_VALUE);
      Serial.println("");
    
      ADE7878_SPI_WRITE(AIGAIN, AIGAIN_CAL_VALUE, 4);
      ADE7878_SPI_WRITE(AVGAIN, AVGAIN_CAL_VALUE, 4);
      
      Serial.print("  BIRMS Expected = "); Serial.println(Percent_FS_Current * RMS_FS_Codes ,0);
      Serial.print("  BVRMS Expected = "); Serial.println(Percent_FS_Voltage * RMS_FS_Codes ,0);
      Serial.print("  BIRMS RAW = "); Serial.println(ADE7878_SPI_READ(BIRMS, 4), DEC);
      Serial.print("  BVRMS RAW = "); Serial.println(ADE7878_SPI_READ(BVRMS, 4), DEC);
      Serial.println("");
      Serial.print("  BIGAIN_CAL_VALUE "); Serial.println(BIGAIN_CAL_VALUE);
      Serial.print("  BVGAIN_CAL_VALUE "); Serial.println(BVGAIN_CAL_VALUE);
      Serial.println("");
    
      ADE7878_SPI_WRITE(BIGAIN, BIGAIN_CAL_VALUE, 4);
      ADE7878_SPI_WRITE(BVGAIN, BVGAIN_CAL_VALUE, 4);
    
    
      Serial.print("  CIRMS Expected = "); Serial.println(Percent_FS_Current * RMS_FS_Codes ,0);
      Serial.print("  CVRMS Expected = "); Serial.println(Percent_FS_Voltage * RMS_FS_Codes ,0);
      Serial.print("  CIRMS RAW = "); Serial.println(ADE7878_SPI_READ(CIRMS, 4), DEC);
      Serial.print("  CVRMS RAW = "); Serial.println(ADE7878_SPI_READ(CVRMS, 4), DEC);
      Serial.println("");
      Serial.print("  CIGAIN_CAL_VALUE "); Serial.println(CIGAIN_CAL_VALUE);
      Serial.print("  CVGAIN_CAL_VALUE "); Serial.println(CVGAIN_CAL_VALUE);
      Serial.println("");
    
      ADE7878_SPI_WRITE(CIGAIN, CIGAIN_CAL_VALUE, 4);
      ADE7878_SPI_WRITE(CVGAIN, CVGAIN_CAL_VALUE, 4);
    
    
    
      ADE7878_SPI_WRITE(LINECYC, (accumulation_time / (1.00 / Line_Freq / 2)), 2); // 300 half linecycles or 3 sec at 50Hz  360 half line cycles at 60hz for 3 sec
    
      Serial.print("  LINECYCLES for "); Serial.print(accumulation_time); Serial.print(" SEC accumulation time = "); Serial.println(accumulation_time / (1.00 / Line_Freq / 2), 0);
    
      IRMS_LSB = I_TEST / (RMS_FS_Codes * Percent_FS_Current);
      VRMS_LSB = V_TEST / (RMS_FS_Codes * Percent_FS_Voltage);
      WATT_LSB = (V_TEST * I_TEST) / (PMAX * Percent_FS_Current * Percent_FS_Voltage / pow(2,4) ) ; // register is 2^4 smaller the output of LPF
    
    //<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<
    
      //Or KWH/LSB can be calculated by using expected values and the signal chain. (watthr over accumulation time) / (calculated watthr register over accumulation time )// note accumulation time cancels out I left it in for clarity
      
      WH_LSB = ((double)(((V_TEST * I_TEST * Power_factor) / 3600) * accumulation_time) / (((double)(PMAX * Percent_FS_Current * Percent_FS_Voltage  * 8000 * accumulation_time )) / ((double)(WTHR_Value)))); // (watthr over accumulation time) / (calculated watthr register over accumulation time )
      
    //<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<
    
    
      Serial.println("");
      Serial.print("  IRMS_LSB = "); Serial.println(IRMS_LSB, 8);
      Serial.print("  VRMS_LSB = "); Serial.println(VRMS_LSB, 8);
      Serial.print("  WATT_LSB = "); Serial.println(WATT_LSB, 8);
      Serial.print("  WH_LSB  = "); Serial.println(WH_LSB, 8);
      Serial.println("");
    
      delay(10000);
    
      Serial.println("  Cf will measure 3 x expected CF if 3 phases are preset at same V and I and PF");
      Serial.print("  Cf Frequency Measured By Micro = "); Serial.print(cf_freq, 6); Serial.println(" HZ ");
      Serial.println("");
      Serial.println("");
      while (1) {
        if ( (ADE7878_SPI_READ(STATUS0, 4) & 32) == 32)
        {
          ADE7878_SPI_WRITE(STATUS0, 32, 4);
          
          Serial.print("  Updated Every "); Serial.print(accumulation_time / (1.00 / Line_Freq / 2),0); Serial.println(" Half Lincycles ");
          Serial.println("");
          Serial.print("  AIRMS = "); Serial.print(ADE7878_SPI_READ(AIRMS, 4) * IRMS_LSB,4); Serial.println(" IRMS");
          Serial.print("  AVRMS = "); Serial.print(ADE7878_SPI_READ(AVRMS, 4) * VRMS_LSB,4); Serial.println(" VRMS");
          
          Serial.print("  AWATT = "); Serial.print(Sign_extend(ADE7878_SPI_READ(AWATT, 4)) * WATT_LSB,4); Serial.println(" WATTS"); 
          Serial.print("  AVA   = ");   Serial.print(ADE7878_SPI_READ(AVA, 4) * WATT_LSB,4); Serial.println(" WATTS"); 
          Serial.print("  AVAR  = ");  Serial.print(Sign_extend(ADE7878_SPI_READ(AVAR, 4)) * WATT_LSB,4); Serial.println(" WATTS"); 
    
          Serial.print("  AWATTHR = "); Serial.print(Sign_extend(ADE7878_SPI_READ(AWATTHR, 4)) * WH_LSB/1000,6); Serial.print(" KW / ");Serial.print(accumulation_time);Serial.println(" SEC accumulation");
          Serial.print("  AVAHR   = ");   Serial.print(ADE7878_SPI_READ(AVAHR, 4) * WH_LSB/1000,6); Serial.print(" KW / ");Serial.print(accumulation_time);Serial.println(" SEC accumulation");
          Serial.print("  AVARHR  = ");  Serial.print(Sign_extend(ADE7878_SPI_READ(AVARHR, 4)) * WH_LSB/1000,6); Serial.print(" KW / ");Serial.print(accumulation_time);Serial.println(" SEC accumulation");
          
          Serial.println("");
          Serial.print("  BIRMS = "); Serial.print(ADE7878_SPI_READ(BIRMS, 4) * IRMS_LSB,4); Serial.println(" IRMS");
          Serial.print("  BVRMS = "); Serial.print(ADE7878_SPI_READ(BVRMS, 4) * VRMS_LSB,4); Serial.println(" VRMS");
          
          Serial.print("  BWATT = "); Serial.print(Sign_extend(ADE7878_SPI_READ(BWATT, 4)) * WATT_LSB,4); Serial.println(" WATTS"); 
          Serial.print("  BVA   = ");   Serial.print(ADE7878_SPI_READ(BVA, 4) * WATT_LSB,4); Serial.println(" WATTS"); 
          Serial.print("  BVAR  = ");  Serial.print(Sign_extend(ADE7878_SPI_READ(BVAR, 4)) * WATT_LSB,4); Serial.println(" WATTS"); 
    
          Serial.print("  BWATTHR = "); Serial.print(Sign_extend(ADE7878_SPI_READ(BWATTHR, 4)) * WH_LSB / 1000,6); Serial.print(" KW / ");Serial.print(accumulation_time);Serial.println(" SEC accumulation");
          Serial.print("  BVAHR   = ");   Serial.print(ADE7878_SPI_READ(BVAHR, 4) * WH_LSB/1000,6);Serial.print(" KW / ");Serial.print(accumulation_time);Serial.println(" SEC accumulation");
          Serial.print("  BVARHR  = ");  Serial.print(Sign_extend(ADE7878_SPI_READ(BVARHR, 4)) * WH_LSB/1000,6); Serial.print(" KW / ");Serial.print(accumulation_time);Serial.println(" SEC accumulation");
          
          Serial.println("");
          Serial.print("  CIRMS = "); Serial.print(ADE7878_SPI_READ(CIRMS, 4) * IRMS_LSB,4); Serial.println(" IRMS");
          Serial.print("  CVRMS = "); Serial.print(ADE7878_SPI_READ(CVRMS, 4) * VRMS_LSB,4); Serial.println(" VRMS");
          
          Serial.print("  CWATT = "); Serial.print(Sign_extend(ADE7878_SPI_READ(CWATT, 4)) * WATT_LSB,4); Serial.println(" WATTS"); 
          Serial.print("  CVA   = ");   Serial.print(ADE7878_SPI_READ(CVA, 4) * WATT_LSB,4); Serial.println(" WATTS"); 
          Serial.print("  CVAR  = ");  Serial.print(Sign_extend(ADE7878_SPI_READ(CVAR, 4)) * WATT_LSB,4); Serial.println(" WATTS");
        
          Serial.print("  CWATTHR = "); Serial.print(Sign_extend(ADE7878_SPI_READ(CWATTHR, 4)) * WH_LSB / 1000,6); Serial.print(" KW / ");Serial.print(accumulation_time);Serial.println(" SEC accumulation");
          Serial.print("  CVAHR   = ");   Serial.print(ADE7878_SPI_READ(CVAHR, 4) * WH_LSB/1000,6); Serial.print(" KW / ");Serial.print(accumulation_time);Serial.println(" SEC accumulation");
          Serial.print("  CVARHR  = ");  Serial.print(Sign_extend(ADE7878_SPI_READ(CVARHR, 4)) * WH_LSB/1000,6);Serial.print(" KW / ");Serial.print(accumulation_time);Serial.println(" SEC accumulation");
          
          Serial.println("");
        }
      }
    }
    
    int32_t Sign_extend(int32_t reg_value)
    {
      if (reg_value > 0x800000)
        reg_value = reg_value + 0xFF000000;
        return reg_value;
    }
    
      
    
    
    void ADE7878_reg_config()
    {
     
      
      //ADE7878_SPI_WRITE(AIGAIN, 0x0, 4);
      Serial.print("AIGAIN = ");
      Serial.println(ADE7878_SPI_READ(AIGAIN,4), HEX);
    
      
      //ADE7878_SPI_WRITE(BIGAIN, 0x0, 4);
      Serial.print("BIGAIN = ");
      Serial.println(ADE7878_SPI_READ(BIGAIN,4), HEX);
      
      
      //ADE7878_SPI_WRITE(CIGAIN, 0x0, 4);
      Serial.print("CIGAIN = ");  
      Serial.println(ADE7878_SPI_READ(CIGAIN,4), HEX);
      
      //ADE7878_SPI_WRITE(AVGAIN, 0x0 , 4);
      Serial.print("AVGAIN = ");  
      Serial.println(ADE7878_SPI_READ(AVGAIN,4), HEX);
      
      //ADE7878_SPI_WRITE(BVGAIN, 0x0 , 4);
      Serial.print("BVGAIN = ");  
      Serial.println(ADE7878_SPI_READ(BVGAIN,4), HEX);
      
      //ADE7878_SPI_WRITE(CVGAIN, 0x0 , 4);
      Serial.print("CVGAIN = ");  
      Serial.println(ADE7878_SPI_READ(CVGAIN,4), HEX);
    
      ADE7878_SPI_WRITE(CF1DEN, 0x64 ,2);
      Serial.print("CF1DEN = ");  
      Serial.println(ADE7878_SPI_READ(CF1DEN,2), HEX);
    
      ADE7878_SPI_WRITE(CF2DEN, 0x64 ,2);
      Serial.print("CF2DEN = ");  
      Serial.println(ADE7878_SPI_READ(CF2DEN,2), HEX);
    
      ADE7878_SPI_WRITE(CF3DEN, 0x64 ,2);
      Serial.print("CF3DEN = ");  
      Serial.println(ADE7878_SPI_READ(CF3DEN,2), HEX);
    
      ADE7878_SPI_WRITE(WTHR0, 0xFF6A6B ,4);
      Serial.print("WTHR0 = ");  
      Serial.println(ADE7878_SPI_READ(WTHR0,4), HEX);
    
       ADE7878_SPI_WRITE(WTHR1, 0x01 ,4);
      Serial.print("WTHR1 = ");  
      Serial.println(ADE7878_SPI_READ(WTHR1,4), HEX);
    
      ADE7878_SPI_WRITE(VARTHR0, 0xFF6A6B ,4);
      Serial.print("VARTHR0 = ");  
      Serial.println(ADE7878_SPI_READ(VARTHR0,4), HEX);
    
       ADE7878_SPI_WRITE(VARTHR1, 0x01 ,4);
      Serial.print("VARTHR1 = ");  
      Serial.println(ADE7878_SPI_READ(VARTHR1,4), HEX);
    
       ADE7878_SPI_WRITE(VATHR0, 0xFF6A6B ,4);
      Serial.print("VATHR0 = ");  
      Serial.println(ADE7878_SPI_READ(VATHR0,4), HEX);
    
      ADE7878_SPI_WRITE(VATHR1, 0x01 ,4);
      Serial.print("VATHR1 = ");  
      Serial.println(ADE7878_SPI_READ(VATHR1,4), HEX);
    
    
     
      //ADE7878_SPI_WRITE(MASK0, 0x20000, 4); //write run bit
      Serial.print("MASK0 = ");  
      Serial.println(ADE7878_SPI_READ(MASK0,4), HEX);
    
      ADE7878_SPI_WRITE(CFMODE, 0x88, 2); //write run bit
      Serial.print("cfmode = ");  
      Serial.println(ADE7878_SPI_READ(CFMODE,2), HEX);
    
      ADE7878_SPI_WRITE(LCYCMODE, 0xF, 1); //set to use phase a zero crosses for linecycle accumulation
      Serial.print("cfmode = ");  
      Serial.println(ADE7878_SPI_READ(LCYCMODE,1), HEX);
    
      
      ADE7878_SPI_WRITE(RUN, 0x0001, 2); //write run bit
      Serial.print("RUN = ");  
      Serial.println(ADE7878_SPI_READ(RUN,2), HEX);
    }
    
    void READ_RMS_ENERGIES_PRINT()
    {
    
      Serial.print("AIRM = ");
      Serial.print(ADE7878_SPI_READ(AIRMS,4)*IRMS_LSB, DEC);
      Serial.print("  BIRM = ");
      Serial.print(ADE7878_SPI_READ(BIRMS,4)*IRMS_LSB, DEC);
      Serial.print("  CIRMS =  ");
      Serial.print(ADE7878_SPI_READ(CIRMS,4)*IRMS_LSB, DEC);
      Serial.print("  AVRMS =  ");
      Serial.print(ADE7878_SPI_READ(AVRMS,4)*VRMS_LSB, DEC);
      Serial.print("  BVRMS =  ");
      Serial.print(ADE7878_SPI_READ(BVRMS,4)*VRMS_LSB, DEC);
      Serial.print("  CVRMS =  ");
      Serial.print(ADE7878_SPI_READ(CVRMS,4)*VRMS_LSB, DEC);
      Serial.print("  AWATT =  ");
      Serial.print(ADE7878_SPI_READ(AWATT,4)*16* WATT_LSB, HEX);
      Serial.print("  BWATT =  ");
      Serial.print(ADE7878_SPI_READ(BWATT,4)*16* WATT_LSB, HEX);
      Serial.print("  CWATT =  ");
      Serial.print(ADE7878_SPI_READ(CWATT,4)*16* WATT_LSB, HEX);
      Serial.print(" ");
      Serial.println(" ");
      
    }
    
    
    
    
    
    
    void ADE7878_SPI_WRITE(uint16_t Address , uint32_t Data , uint8_t Number_of_bytes)
    {
      uint8_t mhb = 0, hb = 0, mb = 0, lb = 0, p = 0;
      uint32_t j;
    
      j = Data & 0xff;
      lb = j;
      j = (Data & 0xff00) >> 8;
      mb = j;
      j = (Data & 0xff0000) >> 16;
      hb = j;
      j = (Data & 0xff000000) >> 24;
      mhb = j;
    
    
      digitalWrite(SSB_A, LOW);   //set csb low
    
    
      data = SPI.transfer(0x00);  // send address with read bit modified
    
      data = SPI.transfer((Address & 0xFF00) >> 8);      // send upper address with write bit modified
    
      data = SPI.transfer(Address & 0xFF);       // send lower address with write bit modified
    
      //send requested number of bytes
      switch (Number_of_bytes) {
        case 4:
          data = SPI.transfer(mhb);
        case 3:
          data = SPI.transfer(hb);
        case 2:
          data = SPI.transfer(mb);
        case 1:
          data = SPI.transfer(lb);
    
        default:
          break;
      }
    
      digitalWrite(SSB_A, HIGH);  //set csb high
    }
    
    
    
    
    
    // ADE7878_SPI_READ is working~ 7/7/15
    uint32_t ADE7878_SPI_READ (uint16_t Address, uint8_t Number_of_bytes)
    {
      uint8_t mhb = 0, hb = 0, mb = 0, lb = 0;
      uint32_t j;
    
    
      digitalWrite(SSB_A, LOW);   //set csb low
    
    
      data = SPI.transfer(0x01);  // send address with read bit modified
    
      data = SPI.transfer((Address & 0xFF00) >> 8);      // send upper address with write bit modified
    
      data = SPI.transfer(Address & 0xFF);       // send lower address with write bit modified
    
    
      hb = 0;
    
      switch (Number_of_bytes) {
        case 4:
          mhb = SPI.transfer(0x0);   // dummy write
        case 3:
          hb = SPI.transfer(0x0);
        case 2:
          mb = SPI.transfer(0x0);
        case 1:
          lb = SPI.transfer(0x0);
        default:
          break;
      }
    
      digitalWrite(SSB_A, HIGH);  //set csb high
    
      j = mhb << 24;
      j = j + (hb << 16);
      j = j + (mb << 8);
      j = j + lb;
      return j;
    }
    

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.