UG-1098: ADE9000 3-wire delta service confusing image

Hello,

Could anyone please confirm if Figure 66 of UG-1086 (page 47) is wrong? 

It says (see image attached) "Alternatively, a series impedance can be used on Phase B, as shown in Figure 66", but Figure 66 is the same as Figure 64.
If Figure 66 is wrong, how should be the connection of a 3-wire delta service with isolated power supply?

Also I noticed that at the beginning of page 45 it is mentioned "VCONSEL[2:0] = 00" but it is supposed to have 3 bits instead of 2.

In page 49 Table 28 it seems theres a '-' missing:



Image attached with '-' missing
[edited by: NicolasEch at 6:50 PM (GMT 0) on 12 Aug 2020]
Parents Reply Children
No Data