Post Go back to editing

3-Phase 4-wire in to 3-Phase 3 Wire

Thread Summary

The user asked how to configure ADE7878 for 3-phase 4-wire to 3-phase 3-wire connections. The final answer provided detailed diagrams and configuration settings from AN-639 and the ADE7878 data sheet, emphasizing that phase B must be used as a reference for 3-wire delta connections, not phase C. The CONSEL bits in the ACCMODE register must be set correctly for the desired configuration.
AI Generated Content
  • Good Afternoon

    The ADE7878 can be configured to accept multiple different configurations including 3 phase 4 wire and 3 phase 3 wire wye and delta.  Our FAQ:  AN-639 that is available on our website has detailed diagrams of each connection on pages 12 and 13.  Although these diagram specifically show an older device, the ADE7754, the connections for the ADE78xx are the same.  The one exception to this is the 3 wire delta case where when using the ADE7878 phase B must be used as a reference and not phase C as shown in figure 8.

    When selecting the different configuration the CONSEL bits in the ACCMODE register must be configured to the correct setting.  This is shown in the attached table and further details can be found on page 48 of the ADE7878 data sheet..

    Kind Regards

    aritchie

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.