Post Go back to editing

BMS with Li-Battery

Hi

I am going to develop a standalone system and use Li-ion battery for the power source.

In addition, I need to connect several packs of Li-ion battery in parallel to maximize the standby period.

(P.S, in this system, there is no charging functions as the batteries will be received  for charging.)

And my concern is the system should be implemented a battery management system for a batter energy control and safety.

Safety is the mainly concerning point as I think it is dangerous to connect those packs of batteries in parallel, am I right?

Is there any controlling ICs or circuits of such kind of BMS?

I have no ideas for that...

Regards

KaHo

Parents
  • If there is no charging you could connect each pack through a suitable diode to a common battery rail.  This would prevent one pack charging another should they be charged to different levels or of a different age.  I would suggest that each pack makes use of monitoring such as the solutions Luca suggested, particularly with regard to monitoring the stack current, voltage and temperature.  Should any pack experience over discharge, increased temperature or exceed its discharge current specification it should be disconnected from the circuit.

Reply
  • If there is no charging you could connect each pack through a suitable diode to a common battery rail.  This would prevent one pack charging another should they be charged to different levels or of a different age.  I would suggest that each pack makes use of monitoring such as the solutions Luca suggested, particularly with regard to monitoring the stack current, voltage and temperature.  Should any pack experience over discharge, increased temperature or exceed its discharge current specification it should be disconnected from the circuit.

Children
No Data