Hello everyone,
we are experiencing some problems with SPI communication between a STM32F4 MCU and an ADE7868A.
The connection is straight between MISO, MOSI, SCK, /SS, /RESET.
We do what follows:
Set /SS high
Reset the ADE7868 toggling low /RESET for 5ms
Wait 60ms
Set /SS low then high for 3 times with a 5ms period
then while(1)
{
Write via SPI 0x0 in the CONFIG2 register at a speed of 650Khz more or less (we tried other speeds, too)
Read back CONFIG2
Read a register got from the datasheet
}
We get something on the MISO pin that is compatible with a SPI answer but checking with a scope its Vpp (V peak to peak) excursion is very narrow (300mV) and oscillates around 3.3V, never going to GND.
If we pull-down the MISO, it always remains to GND.
We observed the same behaviour on 2 different boards.
The ADE7868A seems to be running as VREF is correct and the crystal oscillates fine. Moreover, the IRQ gets asserted upon reset.
With the oscilloscope we verified the other pins and they behave as expected: data are transmitted correctly to the ADE.
PSM0 is selected, so no power saving is active.
Any ideas?
Thanks