Hello all.
Is this crystal suited to drive the ADE7903 XTAL pins?
DigiKey Part Number: XC1260CT-ND
If not, what is the recommend part?
Best Regards
ADE7903
Production
The ADE7903 is a nonisolated, 3-channel, Σ-Δ analog-to-digital converter (ADC) for the neutral line of polyphase energy
metering applications using shunt...
Datasheet
ADE7903 on Analog.com
Hello all.
Is this crystal suited to drive the ADE7903 XTAL pins?
DigiKey Part Number: XC1260CT-ND
If not, what is the recommend part?
Best Regards
Hi Niolp,
The crystal we use on the evaluation board has a DigiKey Part Number of X1089-ND and I would recommend using this crystal.
The specifications of the crystal you mention look to be very similar to the recommended one, therefore even the one you mention should be ok. The recommended one above has been used with the ADE7903 with no issues.
Regards,
Dlath
Thank you dlath!
I have a few other questions about the ADE7903.
1) For a single phase meter, what type of shunt resistor should i use (regular two lead resistor, 4 lead or kelvin configuration) in order to sense current?
2) Is it necessary to create a voltage divider between neutral and phase wires to satisfy the 500mV input voltage in V1P? or if i follow the test circuit stated in the datasheet with those three resistor in series is enough?
3) Are the diodes(TS4148) needed for normal operation of the circuit, or those are for testing only?
Thank you for your time.
P.S.: I'm not sure if i can ask these question's here in this thread, or if i have to create another one.
Best Regards,
Nuno