Post Go back to editing

ADE7903

1) For a single phase meter, what type of shunt resistor should i use (regular two lead resistor, 4 lead or kelvin configuration) in order to sense current? Can you provide the part used with the evaluation kit?

2) Is it necessary to create a voltage divider between neutral and phase wires to satisfy the 500mV input voltage in V1P? or if i follow the test circuit stated in the datasheet with those three resistor in series is enough?

3) Are the diodes(TS4148) needed for normal operation of the circuit, or those are for testing only?

Thank you for your time.

 

Best Regards,

Nuno

  • Hi Nuno

    Please find my responses below:

    1. The Evaluation board does not have any shunts on it. While performing system level tests using the evaluation board, external shunts must be used. However, you can find a couple of important specs below, that you should look for, in a shunt’s datasheet:

        i) The resistance value of the shunt will mainly depend on the maximum application load current. The signal going into the ADE7903 IC must be within the full-scale range of the ADCs (+31.25mVpeak). For safety, I would back up by some margin from the full-scale level, i.e., setting the application maximum current level to say, ½ full scale.

        ii) The temperature co-efficient of the shunt is another important aspect. You should pick one, whose resistance value doesn’t vary too much with temperature. The gain drift specs for the current and voltage channels are provided in the ADE7903 datasheet. Using these values, you can see if the shunt’s drift will satisfy the system level requirements for accuracy.

    2. Yes. Voltage divider needs to be used to step down the voltage level. The three series resistors (that you refer to) form a divider network along with the 1kohm resistor (Refer to page 11 of Rev.0 datasheet). Any doubts on this still?

    3. The diodes are used in the evaluation board for over-voltage protection- to make sure that the IC isn't damaged due to some large signals (> +2V: Absolute max ratings) entering the IC pins. If this sort of protection is taken care of at the meter level in a different way, then this is not needed.

    Regards

    hmani

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.