ADE7880 ARDUINO CODE EXAMPLES

Hello,

I have ADE7880  and  i need to take voltage (rms value), current (rms value), power and power factor from ADE into the ARDUINO MEGA 2560.

I want to talk a little what i try to do. First i have asynchronous motor and i try to analyze this motor about its efficiency. So i need voltage ,current, power ,and power factor of this motor's input circuit and then take into  these values on MEGA 2560, after this, i will do some calculations with these values then i will show efficiency of motor momentarily on my pc with using c#.

So are there any codes for arduino to take these values from ADE7880?

Regards,

Serhat Karaaslan