Dear All,
I’m working on ADE7880 based 3phase 4wire static electricity meter. Meter configuration 240V, 100A Ct ratio = 2500. How to detect missing neutral tampering situation in PSM0 mode. Please give me details
Regard
Rajamani
ADE7880
Production
The ADE7880 is high accuracy, 3-phase electrical energy measurement IC with serial interfaces and three flexible pulse outputs. The ADE7880 device incorporates...
Datasheet
ADE7880 on Analog.com
Dear All,
I’m working on ADE7880 based 3phase 4wire static electricity meter. Meter configuration 240V, 100A Ct ratio = 2500. How to detect missing neutral tampering situation in PSM0 mode. Please give me details
Regard
Rajamani
Hi Rajamani,
To detect a missing Neutral situation you will need to monitor the voltage, if the RMS voltage goes lower then it should for the line (for example less than 10% of Vnom) and there is still RMS current being measured then this would be a missing neutral situation. On the ADE7880 you can set a voltage sag threshold. Just make sure the ADE7880 does not lose power so that the RMS can be monitored.
Regards,
Dlath
Dear Dlath,
I checked But not working.It is very urgent one. voltage sag used under and over voltage temper
Normal Input (with neutral wire):
ADE value.
R phase = 240.01v and 5A
Y phase = 240.03v and 5A
B phase = 240.01v and 5A
Without Neutral wire:
DE value
R phase = 250.9v and 5A
Y phase = 238.02v and 5A
B phase = 236.76v and 5A
Each and every phase different voltage. How can i detect a missing Neutral situation
Hi Rajamani,
I can suggest two more options and you can check which one works for you.
Regards,
Dlath
Hello dlath,
We are also trying to detect Neutral loss using ADE7880. As suggested above, we tried reading ANGLEx register when neutral loss is simulated. But the values in ANGLEx registers does not change much to differentiate neutral loss from normal condition. We normally(without neutral loss) got the readings as <RY = 116, <YB = 122, and <RB = 122, hence we are unable to identify. Is there any other way to differentiate neutral loss?
Thanks and Regards,
Omkar