Energy Monitoring and Metering in VFD Output 0 to 200 Hz

For a project to register voltages, currents and power at the output of power VFD (100 to 1100 KVA) used in ALS for the oil industry, I need an ADE series chip or another serious one that can process line frequency frequencies. 0 to 200 Hz. If it is not possible, you could tell me what measurements I can do within this range with an ADE7880, even if it is using some compensation factor.