I know ADE7751 has a bandwidth of 14 khz and a oversampling rate of 900 khz. And I also have a sample rate of 4.8 KHZ. I wanna know how the sampling rate is calculated. 

Does someone know about this ? Any reply will be appreciated
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADE7751
Production
The ADE7751 is an accurate fault tolerant electrical energy measurement IC intended for use in two-wire distribution systems. It provides instantaneous...
Datasheet
ADE7751 on Analog.com
I know ADE7751 has a bandwidth of 14 khz and a oversampling rate of 900 khz. And I also have a sample rate of 4.8 KHZ. I wanna know how the sampling rate is calculated. 

Does someone know about this ? Any reply will be appreciated
Hi,
I'll be moving this thread to its proper community https://ez.analog.com/energy-metering/. Someone here may be able to assist you.
Thanks,
Jellenie
Hi Lynne,
The ADE7751 is a metering IC for AC energy.
Current and voltage channel sample rate of the Sigma delta ADC is clk/4 or 3.579Mhz/4 or 894750Khz.
The Anti-alias and the internal Sync filter determine the measurement bandwidth 14Khz.
Voltage channel is multiplied by the current channel internally accumulated and a digital to Freq conversion is done to create a pulse output proportional to AC Energy.
This is not an ADC. You have no way to read ADC samples. All you get is a CF (calibration Frequency).
Can you explain what you are trying to do?
Dave
Hi Dave,
Thanks for your reply. I only know that the sampling rate is 4.8Khz and the metering IC is the ADE7751. I wanna know that how can I calculate the sampling rate. Could you help me out and tell me the formula? I will be deeply grateful.
Lynne
Hi Lynne,
I am still not sure what you are asking for. The adc sample rate is based on the crystal input /4 3.579Mhz/4 or 894750Khz.
Can you show me a schematic of what you are trying to do with input signals and output signals?and where does the 4.8Khz sample rate come from?
Dave
Hi Dave,
Thank you for your reply. I'm sorry that I don't have the schematic of what I am trying to do with input signals and output signals. My customer gave me a picture and asked me how could he get 4.8khz. I only know that the metering IC is ADE7751 and I don't have any information about this. 
Lynne
Hi Lynne,
The important information is the 3200imp/Kwh. This is the meter constant and used to calibrate the meter. In this case I am guessing the ADC used has a sampling rate of 4.8Khz. The ADE7751 samples at the crystal /4 or 894750Khz the sync output bandwith is 14Khz. The ADE7751 has a higher sample rate than 4.8Khz so you will be able to measure the same information.
You should not focus on the 4.8Khz so much. I think this number is indicating how may harmonics the meter can measure. The ADE7751 can measure the required harmonics with a 14khz bandwidth.
This will help you design a meter with the ADE7751
https://www.analog.com/media/en/technical-documentation/application-notes/AN-574.pdf
based on your photo these are you values.
V= 230V
I=5 amps nominal (IB) and (40) Max
50Hz
3200imp/KWH
Dave
Hi Lynne,
The important information is the 3200imp/Kwh. This is the meter constant and used to calibrate the meter. In this case I am guessing the ADC used has a sampling rate of 4.8Khz. The ADE7751 samples at the crystal /4 or 894750Khz the sync output bandwith is 14Khz. The ADE7751 has a higher sample rate than 4.8Khz so you will be able to measure the same information.
You should not focus on the 4.8Khz so much. I think this number is indicating how may harmonics the meter can measure. The ADE7751 can measure the required harmonics with a 14khz bandwidth.
This will help you design a meter with the ADE7751
https://www.analog.com/media/en/technical-documentation/application-notes/AN-574.pdf
based on your photo these are you values.
V= 230V
I=5 amps nominal (IB) and (40) Max
50Hz
3200imp/KWH
Dave
Hi Dave,
Thanks for your reply.I will refer to the link you sent me.And thank you so much for your assistance.
Lynne