Dear All,
Can anyone provide the information about measuring voltage and frequency in 400 Hz line systems. That is, Can we use ADE7752 or any other 3 phase IC with 400 Hz - 3 Phase - 115 VAC system without building any external circuits?
Regards,
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADE7752
Obsolete
The ADE7752 is an accurate active energy measurement IC intended for use in any 3-phase distribution system. It provides instantaneous and average real...
Datasheet
ADE7752 on Analog.com
Dear All,
Can anyone provide the information about measuring voltage and frequency in 400 Hz line systems. That is, Can we use ADE7752 or any other 3 phase IC with 400 Hz - 3 Phase - 115 VAC system without building any external circuits?
Regards,
Hi igg,
The ADE chips supports 50 Hz, 60 Hz standard frequencies of electrical power. It is possible, BUT, we cannot guarantee the accuracy based on the specs on a frequency of 400 Hz, and we may not recommend it. The ADE chips are designed for metering and non utility applications for energy measurement on electrical lines supporting the 50 Hz/60 Hz standard.
A workaround in the ADE chip is to interpret the 400 Hz as a part of its harmonic (of the 50Hz fundamental), like the ADE7880 which has a harmonic engine BUT I think this is not the best option to do.
Thank you very much.