Post Go back to editing

ADM1178 I2C Read

Hi,

sending a single  I2C write command to the ADM1178 works as expected. The ADM1178 returns the ACK as one would expect. If an individual read command is sent, three bytes can be successfully read back, thus it also works as expected.

However when a write command (Start - ADR - W - Data -  Stop) is immediately (> 10us) followed  by a read (start - ADR -  R) the ADM1178 does not send an ACK after the address byte and Read command were sent.

Sending two consecutive write commands (spaced 10us apart  works as expected also (meaning the ADM1178 acknowledges every write command).

Are there any special timing conditions that need to be met in order to send an read instruction immediately after a write cmd ?

thanks

Oliver

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.