Post Go back to editing

Video Capture: adi_dev_Video_Open failed error

We have a ADZS-BF707-BLIP2 board to demonstrate VOS functionality but there is an error occurring with it and I cannot obtain any image in any of three different computers I tested it, although it has worked before.

The returning error is ‘ERROR: Video Capture: adi_dev_Video_Open failed’ as in the attached compacted image. This message occurs no matter the chosen sensor (omnivision or Aptina) nor the flashed application (VOS indoor or VOS outdoor), always using the GUI application.

What could I try to put this board back to work?

Parents
  • Hi,

    I've installed BSP again and error persists. Even with another example, FrameCapture_ClassDriver_OV7692, it got an error when executing 'adi_dev_Video_Open' function.

    One thing I noticed, but it doesn't seem to be related to this problem, are some warnings during loading the firmware through CCES and emulator, as copied below. I've already tried emulator and Flash runs.

    ERROR: [Error xml1013] [emulator] Unable to process custom action for register "DMC0_PHY_CTL1" in custom board file "C:\Documents and Settings\Administrador\cces\2.0.0\examples\bf707_blip2_1.0.0\Power_On_Self_Test\ADZS-BF707-BLIP2-proc.xml", because there already exists a register definition for name "DMC0_PHY_CTL1". You cannot modify a register from the base processor definition and any additional custom registers must be uniquely named.

    ERROR: [Error xml1013] [windows creation] Unable to process custom action for register "DMC0_PHY_CTL1" in custom board file "C:\Documents and Settings\Administrador\cces\2.0.0\examples\bf707_blip2_1.0.0\Power_On_Self_Test\ADZS-BF707-BLIP2-proc.xml", because there already exists a register definition for name "DMC0_PHY_CTL1". You cannot modify a register from the base processor definition and any additional custom registers must be uniquely named.

    Loading application: "C:\Documents and Settings\Administrador\cces\2.0.0\examples\bf707_blip2_1.0.0\FrameCapture_ClassDriver_OV7692\Debug\FrameCapture_ClassDriver_OV7692.dxe"

    ERROR: [Error xml1013] [windows creation] Unable to process custom action for register "DMC0_PHY_CTL1" in custom board file "C:\Documents and Settings\Administrador\cces\2.0.0\examples\bf707_blip2_1.0.0\Power_On_Self_Test\ADZS-BF707-BLIP2-proc.xml", because there already exists a register definition for name "DMC0_PHY_CTL1". You cannot modify a register from the base processor definition and any additional custom registers must be uniquely named.

    Load complete.

    Core clock:      384000000 Hz

    System clock:    192000000 Hz

    System clock 0:   96000000 Hz

    System clock 1:  192000000 Hz

    adi_dev_Video_Open failed

    Error in configuring the sensor.

Reply
  • Hi,

    I've installed BSP again and error persists. Even with another example, FrameCapture_ClassDriver_OV7692, it got an error when executing 'adi_dev_Video_Open' function.

    One thing I noticed, but it doesn't seem to be related to this problem, are some warnings during loading the firmware through CCES and emulator, as copied below. I've already tried emulator and Flash runs.

    ERROR: [Error xml1013] [emulator] Unable to process custom action for register "DMC0_PHY_CTL1" in custom board file "C:\Documents and Settings\Administrador\cces\2.0.0\examples\bf707_blip2_1.0.0\Power_On_Self_Test\ADZS-BF707-BLIP2-proc.xml", because there already exists a register definition for name "DMC0_PHY_CTL1". You cannot modify a register from the base processor definition and any additional custom registers must be uniquely named.

    ERROR: [Error xml1013] [windows creation] Unable to process custom action for register "DMC0_PHY_CTL1" in custom board file "C:\Documents and Settings\Administrador\cces\2.0.0\examples\bf707_blip2_1.0.0\Power_On_Self_Test\ADZS-BF707-BLIP2-proc.xml", because there already exists a register definition for name "DMC0_PHY_CTL1". You cannot modify a register from the base processor definition and any additional custom registers must be uniquely named.

    Loading application: "C:\Documents and Settings\Administrador\cces\2.0.0\examples\bf707_blip2_1.0.0\FrameCapture_ClassDriver_OV7692\Debug\FrameCapture_ClassDriver_OV7692.dxe"

    ERROR: [Error xml1013] [windows creation] Unable to process custom action for register "DMC0_PHY_CTL1" in custom board file "C:\Documents and Settings\Administrador\cces\2.0.0\examples\bf707_blip2_1.0.0\Power_On_Self_Test\ADZS-BF707-BLIP2-proc.xml", because there already exists a register definition for name "DMC0_PHY_CTL1". You cannot modify a register from the base processor definition and any additional custom registers must be uniquely named.

    Load complete.

    Core clock:      384000000 Hz

    System clock:    192000000 Hz

    System clock 0:   96000000 Hz

    System clock 1:  192000000 Hz

    adi_dev_Video_Open failed

    Error in configuring the sensor.

Children
No Data