Post Go back to editing

Video Capture: adi_dev_Video_Open failed error

We have a ADZS-BF707-BLIP2 board to demonstrate VOS functionality but there is an error occurring with it and I cannot obtain any image in any of three different computers I tested it, although it has worked before.

The returning error is ‘ERROR: Video Capture: adi_dev_Video_Open failed’ as in the attached compacted image. This message occurs no matter the chosen sensor (omnivision or Aptina) nor the flashed application (VOS indoor or VOS outdoor), always using the GUI application.

What could I try to put this board back to work?

Parents
  • Hi,

    I am afraid this looks like an issue with the BLIP board hardware. However just to ensure that the library was not modified can you run a fresh install of the BSP package and then try running IOS/VOS and see if this issue is replicable?

    Were you running with an emulator or through Flash earlier?. Can you try writing the latest dxe from AdVision Sensor 1.0.2 to flash to see if you still get this error?. The Users Guide will have instructions on writing the dxe to flash.

    Regards,

    Neeraj

Reply
  • Hi,

    I am afraid this looks like an issue with the BLIP board hardware. However just to ensure that the library was not modified can you run a fresh install of the BSP package and then try running IOS/VOS and see if this issue is replicable?

    Were you running with an emulator or through Flash earlier?. Can you try writing the latest dxe from AdVision Sensor 1.0.2 to flash to see if you still get this error?. The Users Guide will have instructions on writing the dxe to flash.

    Regards,

    Neeraj

Children
No Data