Post Go back to editing

Fine tune the parameters of People counter

Dear Sir,

After I tested the ADVisionSensorController GUI, I don’t know how to fine tune the setting of PPLCNTR configuration, Can you teach me how to setting those parameters? Especially at Detect Rate, Size of person, Foreground blobs, Object size, Threshold, Pixel Percentage Threshold parameters.

Thanks.

Best regards.

Ray.

Parents
  • Hi Ray,

    To change any parameter first the analytics shall be in disabled mode. In GUI window under PPLCNTR tab you will see a button Enable VA BLIP. When you click this the application is running and you cannot change these parameters. After enabling the application the button text changes to Disable VA BLIP.

    As of now we do not suggest to change Detect Rate, Threshold, Pixel Percentage Threshold and Object Size.

    To enable Foreground Blobs change the value in the text box next to it to 1. After this when the user clicks on Enable VA BLIP you can see that the blobs detected by the application are drawn on the Video window.

    To change size of person, please refer to the user guide which is accessible when you click on GUI User's Guide option under the Help tab of the GUI.

    Thank You & Regards,

    Sudheer

Reply
  • Hi Ray,

    To change any parameter first the analytics shall be in disabled mode. In GUI window under PPLCNTR tab you will see a button Enable VA BLIP. When you click this the application is running and you cannot change these parameters. After enabling the application the button text changes to Disable VA BLIP.

    As of now we do not suggest to change Detect Rate, Threshold, Pixel Percentage Threshold and Object Size.

    To enable Foreground Blobs change the value in the text box next to it to 1. After this when the user clicks on Enable VA BLIP you can see that the blobs detected by the application are drawn on the Video window.

    To change size of person, please refer to the user guide which is accessible when you click on GUI User's Guide option under the Help tab of the GUI.

    Thank You & Regards,

    Sudheer

Children
No Data