Post Go back to editing

Fine tune the parameters of People counter

Dear Sir,

After I tested the ADVisionSensorController GUI, I don’t know how to fine tune the setting of PPLCNTR configuration, Can you teach me how to setting those parameters? Especially at Detect Rate, Size of person, Foreground blobs, Object size, Threshold, Pixel Percentage Threshold parameters.

Thanks.

Best regards.

Ray.

  • Hi Ray,

    To change any parameter first the analytics shall be in disabled mode. In GUI window under PPLCNTR tab you will see a button Enable VA BLIP. When you click this the application is running and you cannot change these parameters. After enabling the application the button text changes to Disable VA BLIP.

    As of now we do not suggest to change Detect Rate, Threshold, Pixel Percentage Threshold and Object Size.

    To enable Foreground Blobs change the value in the text box next to it to 1. After this when the user clicks on Enable VA BLIP you can see that the blobs detected by the application are drawn on the Video window.

    To change size of person, please refer to the user guide which is accessible when you click on GUI User's Guide option under the Help tab of the GUI.

    Thank You & Regards,

    Sudheer

  • Hi Ray,

    The default values are Object Size 0x320, Threshold: 0xC8 and Pixel percentage threshold is 0x23.

    If you have modified several parameters and not deleted any settings from ManagerFiles, then restarting the GUI shall do the reloading of the default values.

    Regards,

    Sudheer

  • Hi Sudheer,

    Thanks so much your reply, Because I modified the parameters many times to try performance, and I don't know the default value, Could you help to show the default value of parameters?

    Thanks and Best regards.

    Ray.

  • Hi Sudheer,

    Thanks so much.

    Best regards.

    Ray.

  • Hi Ray,

    Can you mark the appropriate thread as Answered / Helpful.

    Regards,

    Sudheer

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.