Post Go back to editing

Over the air (OTA) updates for EagleEye

Thread Summary

The user inquired about upgrading the algorithm in the field for ADI EagleEye PeopleCount software. The final answer confirmed that firmware upgrades are supported and can be performed using APIs detailed in the AN-FirmwareUpgradeEagleEyePeopleCount document, which includes example Python scripts. For the scripts, the user should contact eagleeye.support@analog.com.
AI Generated Content
Parents
  • ADI EagleEye PeopleCount software supports firmware upgrades in the field. If you plan to connect your MCU to ADI EagleEye DSP, then you can use the APIs listed in the document AN-FirmwareUpgradeEagleEyePeopleCount.doc. It comes with example python scripts that can be used to upgrade firmware and it is a very simple example code. If you need the python scripts, please send an email requesting them to eagleeye.support@analog.com .

Reply
  • ADI EagleEye PeopleCount software supports firmware upgrades in the field. If you plan to connect your MCU to ADI EagleEye DSP, then you can use the APIs listed in the document AN-FirmwareUpgradeEagleEyePeopleCount.doc. It comes with example python scripts that can be used to upgrade firmware and it is a very simple example code. If you need the python scripts, please send an email requesting them to eagleeye.support@analog.com .

Children
No Data