Post Go back to editing

Reading output data from EagleEye device

Thread Summary

The user inquires about methods to connect to ADI EagleEye PeopleCount and retrieve output data. The final answer indicates that firmware upgrades for ADI EagleEye PeopleCount can be performed in the field using APIs detailed in the AN-FirmwareUpgradeEagleEyePeopleCount document, which includes example Python scripts for firmware upgrades. For the scripts, users should contact Analog Devices support.
AI Generated Content

I want to learn in detail about the ways I can connect to ADI EagleEyeTM PeopleCount and get the output data.

  • ADI EagleEye PeopleCount software supports firmware upgrades in the field. If you plan to connect your MCU to ADI EagleEye DSP, then you can use the APIs listed in the document AN-FirmwareUpgradeEagleEyePeopleCount.doc. It comes with example python scripts that can be used to upgrade firmware and it is a very simple example code. If you need the python scripts, please send an email requesting them to eagleeye.support@analog.com .