Analog.com
Analog
Dialogue
Wiki
English
Analog.com
Analog
Dialogue
Wiki
简体中文
EngineerZone
Site
Search
User
Site
Search
User
EngineerZone
Search
Log in
Site
Search
Log in
Home
Blogs ⌵
EngineerZone Spotlight
The Engineering Mind
Browse ⌵
All Groups
All Members
Support ⌵
3D ToF Depth Sensing
Amplifiers
Analog Microcontrollers
Audio
Clock and Timing
Data Converters
Design Tools and Calculators
Direct Digital Synthesis (DDS)
Embedded Vision Sensing
Energy Monitoring and Metering
FPGA Reference Designs
Industrial Ethernet
Interface and Isolation
Low Power RF Transceivers
MEMS Inertial Sensors
Motor Control Hardware Platforms
Optical Sensing
Power By Linear
Processors and DSP
Reference Circuits
RF and Microwave
Switches/Multiplexers
Temperature Sensors
Video
Wide Band RF Transceivers
Wireless Sensor Networks Reference Library
My EZ
More
Cancel
主页
浏览 ⌵
收件箱
个人设置
会员
专区列表
论坛专区 ⌵
放大器专区
精密转换器专区
音频专区
ADE电能计量专区
MEMS和传感器专区
接口和隔离专区
Power 中文专区
ADUC微处理器专区
锁相环专区
开关和多路复用器专区
温度传感器
基准电压源专区
资源库
论坛使用指南
技术支持参考库
在线研讨会
论坛社群活动
论坛激励活动
More
Cancel
Processors and DSP
Documents
Can I access variables (in C code) defined in an external memory device
Q&A
Discussions
Documents
File Uploads
Video/Images
Tags
Members
Reports
Managers
More
Cancel
New
Processors and DSP requires membership for participation - click to join
+
Documents
2 video cameras to the video decoder on the ADSP-BF561 Evaluation board?
3 x EEPI on ADSP-BF548 processors?
ADSP-21363: Wants to look it up in a j-tag chain and sitll use J-tag emulater
ADSP-21368 - WS Value
ADSP-21469 questions regarding PCN 11_0097 rev C
ADSp-BF532: I wish to read the odd 8bit registers must I always
ADSP-BF537: Is the BF537 kit able to do promiscuous mode?
ADSP-CM40x feature a Data Cache?
ADSp-TS201S: FFT difference in simulation and rel Time
Are MEMX and MEMY physical memories?
availability of default DSP Boot source code for the TigerSHARC
benchmarks for the TigerSHARC ADSP-TS201 Processor
BF537 supporting 8MB of FLASH?
BF561 SDK 2.01 : JPEG encoding from YUV422 format.
Blackfin CAN Pin operation after power-on
Blackfin processor and intrinsic (built-in) functions?
bus loading with the Blackfin BF533
Call and Jump instructions at the ADSP-TS101S
Can I access variables (in C code) defined in an external memory device
Can I Perform flash programming in SPI Memory Mapped mode?
Can I place DATA in CODE memory and vice-versa?
Can I use MATLAB and Simulink with the ADSP-CM40x and IAR Tool-chain?
CAN issue - remove frames
Changing IP address at run time
Chip Revision identification
Compiler needed for DSP
Configuration for slow Flash devices
connect my Blackfin EZ-Kit to a high speed converter (a few MHz) over the PPI Interface
Connected Devices Virtual Conference
connection of S1D13A05 Epson device to the ADSP-BF537
Core access of same variables at the ADSP-BF561
Count of Blackfin core clock cycles
Difference between SHARED_MEMORY{} and COMMON_MEMORY{} section commands
differences between the ADSP-BF537 and the ADSP-BF533 booting process
Disabling watchdog
DMA error conditions
Does the ADDS-USB-ICE include any software (on disk)
Does the JTAG Reference EE-68 Apply to the Newer Processors?
Driver Type E Specifications Missing from ADSP-BF60x Datasheet
duty cycle of the clock
dynamically turn off and on the instruction and/or data
Enabling Product-Specific Push Notifications from analog.com Web Site
FAQ: Define Nesting Interrupt concepts in Griffin Processor?
FAQ: Floating Power Pins on Processors
FAQ: How to add Compiler options with CCES GUI?
FAQ: How to use preprocessors in script for VDSP++5.0?
FAQ: ICE-1000 emulator does not recognize custom BF board
FAQ: Is available an elfloader.exe for the ADSP-CM408F?
FAQ: Is there a general overview on using the Disassembly window
FAQ: RoHS-Compliant Parts and Pin-Compatibility with Predecessors
floating point operations at Blackfin
free download limitations?
Heat sink recommendation for TigerSHARC ADSP-TS20xS
Hooking up interrupts in VDK for programming with Blackfin processors
Host Memory Mode on Blackfin Processors?
How can I utilize Cache with Async memory connected SRAM?
How can I utilize Cache with Async memory connected SRAM? (1)
How do I connect the Real Time Clock (RTC) pins on Blackfin?
How do I program the Blackfin PLL
How do I validate SPI on my newly designed board based on ADSP-SC58x/ADSP-2158x processors?
How do I validate the SPORT on my newly designed board based on ADSP-SC58x/ADSP-2158x processors?
How do I validate the UART on my newly designed board based on ADSP-SC58x/ADSP-2158x processors?
How do I validate TWI on my newly designed board based on ADSP-SC58x/ADSP-2158x processors?
Information for MPEG-4 for the ADSP-BF561
Intel's PCI_to_PCI bridge (21152) between the ADSP-BF535 and the PCI connector
junction temperature on the ADSP-TS101 TigerSHARC Processor
Link Port Cables for the ADSP-TS101 EZ-Kit Lite
Link Port Devices from ADI connected to the TigerSHARC Link Ports
LTSTAT/LRSTAT should be read twice sequentially to ensure correct value - anomaly 18730
Mobile SDRAM on BF533
MTBF and Other Data Required Data
MTBF of the ADSp-BF537
On-chip flash for ADSP-BF538F and ADSP-BF539F
performance of the Blackfin if program exceeds internal memory
physical address of the TEST_MODES register
Porting a VDK-project from Visual DSP++ 3.5 to 4.0
power-up sequencing for giving 3.3V and 1.2 V input supplies to ADSP-BF536/7
Problems with adequate heel fillets IPC
Problems with emulator session using floating license for VisualDSP++ 4.0?
Problems with the license after PC change
Processor Technical Support
PROCESSORS AND DSP SUPPORT COMMUNITY
prototyping the a ADSP-TS203S design with a ADSP-TS201s or a ADSP-TS202S
PWM example for the 21489 EZ-Kit board - Doesn't Exist
Questions 536 / VDK
RE: MDMA Issue with MPEG4 decoder Library (SR#: 0704922)
RE: Processor Technical Support (SR#: 0607855)
RE: Processor Technical Support (SR#: 0706904)
restrictions when communicating with the EZ kit via USB with no ICE on a test drive
schematic symbol, PCB footprint and layout information for the ADSP-TS201 TigerSHARC Processor Evaluation Board
Serial-termination resistors for the ext memory
solutioon for voice applications
Speech recognition on Blackfin and SHARC
Speeding up flash programming using the command-line device programmer (cldp)
Speex and Vorbis decoders
SPI framesync with /SPISS
SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose?
TRST pin at the EZ-KITs
TS201 CJMP and PC problem
Updating ICE-1000/2000 firmware with OpenOCD
USB Voltage at the ADSF-BF53x USB
Using Flash with the Blackfin
Using the ADSP-BF533/2/1, is it possible to store programm code in SDRAM
Visual DSP++ Load driver error (ADSP-BF561 Flash Driver)
What do I need in order to evaluate the ADSP-CM40x Processors?
What is the EngineerZone URL location?
What is XiP?
Where Can I Find the Most Recent Silicon Revision for Processors and DSPs?
Where I can find information regarding reflow temperature profile for a particular processor?
[Bug Report] Sigma 'Hard Clip' in grown algorithm.
[FAQ] : How to suppress Misra rule checking for a particular file or a function?
Can I access variables (in C code) defined in an external memory device
Q
Can I access variables (in C code) defined in an external memory device (or an
8-bit wide CPLD). Let's say I know that one 16-bit CPLDregister has the address
0x8000000. Can I define this register (REG1) as:
#define REG1 ((volatile unsigned int *)0x8000000)
Can I then assign some content to it, let's say a value of 0x8040 as
*REG1 = 0x8040;
A
Yes, that is correct. The above code snippets will assign a 32-bit variable at
address 0x8000000, and then write 0x00008040 to it. (This example is valid for
an ADSP-21369 SHARC processor, where 0x8000000 is an external SDRAM address.
The principal is the same for all SHARC processors but be sure to use a valid
address.)
adsp-21160m
Share
History
More
Cancel
Comments
Related