Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Other Products Library
    • Precision Technology Signal Chains Library
    • Software Modules and SDKs Library
    • Supervisory Circuits Library
    • Wireless Sensor Networks Library

    Latest Webinars

    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      KCC's Quizzes AQQ297 about taking the right dose of medication

      1. First, the quote of the month: " All my life I though air is free until I bought a bag of chips " - unknown 2. New quiz AQQ297 about taking the right...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    Good Marketing Buzz, But How Do I Start?

    "AD74416H! SWIO! - Configurability! Flexibility! Wow !" Marketing is good at spotlighting key features. What it rarely answers is the practical question...

     

    Incorporating Digital Filter Modelling in LTspice Simulations

    When simulating a circuit in LTspice , the goal is likely to gain insight into the analog behaviors and trade-offs of your circuit. It is also likely that...

    Latest Blogs

    • Charting Calm Seas: Tips for Robust RS-485 Data Transmission
    • Unpacking IEC 61508: Low Complexity versus Type A Made Simple
    • Taming the AI Power Storm: Part 2 of 3
    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
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
Processors & DSP
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Processors & DSP
Processors & DSP
Documents What is XiP?
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADAU 1701: FAQ
  • +ADSP-21160M: FAQ
  • +ADSP-21363: FAQ
  • +ADSP-21368: FAQ
  • +ADSP-21369: FAQ
  • +ADSP-21469: FAQ
  • +ADSP-21489: FAQ
  • +ADSP-2160: FAQ
  • +ADSP-BF522: FAQ
  • +ADSP-BF531: FAQ
  • +ADSP-BF532: FAQ
  • +adsp-bf533: FAQ
  • +ADSP-BF534: FAQ
  • +ADSP-BF535: FAQ
  • +ADSP-BF536: FAQ
  • +ADSP-BF537: FAQ
  • +ADSP-BF538F: FAQ
  • +ADSP-BF539: FAQ
  • +ADSP-BF542: FAQ
  • +ADSP-BF544: FAQ
  • +ADSP-BF561: FAQ
  • +adsp-bf561: FAQS
  • +adsp-bf609: FAQS
  • +ADSP-BF60x: FAQ
  • +ADSP-BF70x: FAQ
  • -ADSP-CM408F: FAQ
    • ADSP-CM40x feature a Data Cache?
    • Are MEMX and MEMY physical memories?
    • Can I Perform flash programming in SPI Memory Mapped mode?
    • Can I place DATA in CODE memory and vice-versa?
    • Can I use MATLAB and Simulink with the ADSP-CM40x and IAR Tool-chain?
    • How can I utilize Cache with Async memory connected SRAM?
    • How can I utilize Cache with Async memory connected SRAM? (1)
    • Is available an elfloader.exe for the ADSP-CM408F?
    • SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose?
    • What do I need in order to evaluate the ADSP-CM40x Processors?
    • What is the EngineerZone URL location?
    • What is XiP?
  • +ADSP-SC58x: FAQ
  • +ADSP-TS001: FAQ
  • +ADSP-TS101S: FAQ
  • +ADSP-TS201S: FAQ
  • +CCES: FAQ
  • +cm40x: FAQ
  • +Command-line device programmer (cldp): FAQS
  • +Compiler: FAQ
  • +Connected Devices Virtual Conference: FAQS
  • +Disassembly Window: FAQ
  • +Enabling Product-Specific Push Notifications: FAQS
  • +ICE-1000: FAQ
  • +JEDEC J-STD-020: FAQ
  • +Misra rule checking: FAQ
  • +Nesting Interrupt: FAQ
  • +Power Domains: FAQ
  • +PROCESSORS AND DSP SUPPORT COMMUNITY: FAQS
  • +Questions 536 / VDK: FAQS
  • +RoHS-Compliant: FAQ
  • +Updating ICE-1000/2000 firmware with OpenOCD: FAQ
  • +VDSP-BLKFN-PC-FULL: FAQ
  • +VDSP-TS-PC-FULL: FAQ
  • +VDSP: FAQ
  • +VISUALAUDIO: FAQ

What is XiP?

Q 

What is XiP?

 

A 

XiP is a mode in Flash memory where one can avoid sending commands, and only
send address. Flash memory must be pre-configured to support this. The SPI
Controller must also be programmed with CMDSKIP option. Since the commands are
always sent in single line (even if Quad/Dual are chosen)  the advantage can be
calculated as follows, for a case of Quad Mode with SPI Clock Freq equal to
SCLK Clock Freq. Total SPI bursts can be obtained if one looks at the Cache
Fill Counter values.
Total Core Clock Cycles with XiP = Total Core Clock Cycles without XiP - ((8 x
Total SPI Bursts x CCLK:SCLK Ratio) - 1)
Note - Even if XiP Mode is not enabled, one can still Execute-In-Place from
Flash memory. The major reason why XiP is called as mode is that, slow flash
devices has to support fast code execution and hence the user is expected to
program the best case features (in this case command skip).

Tags: adsp-cm408f
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • What is XiP?
    stephenv
    XiP is a mode in Flash memory where one can avoid sending commands, and only send address. Flash memory must be pre-configured to support this. The SPI Controller must also be programmed with CMDSKIP option...
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • ADSP-SC58x/2158x SPI XIP - Example code
    Sara Collins
    Attached code is used to configure SPI2 in XIP mode. A known pattern of data is written to SPI flash using the flash programmer code and then the data is read back in memory mapped mode with XIP enabled...
 
Related Content
  • What is XiP?
    stephenv
    XiP is a mode in Flash memory where one can avoid sending commands, and only send address. Flash memory must be pre-configured to support this. The SPI Controller must also be programmed with CMDSKIP option...
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • ADSP-SC58x/2158x SPI XIP - Example code
    Sara Collins
    Attached code is used to configure SPI2 in XIP mode. A known pattern of data is written to SPI flash using the flash programmer code and then the data is read back in memory mapped mode with XIP enabled...