Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Processors & DSP
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Processors & DSP
Processors & DSP
Documents junction temperature on the ADSP-TS101 TigerSHARC Processor
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADAU 1701: FAQ
  • +ADSP-21160M: FAQ
  • +ADSP-21363: FAQ
  • +ADSP-21368: FAQ
  • +ADSP-21369: FAQ
  • +ADSP-21469: FAQ
  • +ADSP-21489: FAQ
  • +ADSP-2160: FAQ
  • +ADSP-BF522: FAQ
  • +ADSP-BF531: FAQ
  • +ADSP-BF532: FAQ
  • +adsp-bf533: FAQ
  • +ADSP-BF534: FAQ
  • +ADSP-BF535: FAQ
  • +ADSP-BF536: FAQ
  • +ADSP-BF537: FAQ
  • +ADSP-BF538F: FAQ
  • +ADSP-BF539: FAQ
  • +ADSP-BF542: FAQ
  • +ADSP-BF544: FAQ
  • +ADSP-BF561: FAQ
  • +adsp-bf561: FAQS
  • +adsp-bf609: FAQS
  • +ADSP-BF60x: FAQ
  • +ADSP-BF70x: FAQ
  • +ADSP-CM408F: FAQ
  • +ADSP-SC58x: FAQ
  • +ADSP-TS001: FAQ
  • -ADSP-TS101S: FAQ
    • availability of default DSP Boot source code for the TigerSHARC
    • Call and Jump instructions at the ADSP-TS101S
    • junction temperature on the ADSP-TS101 TigerSHARC Processor
    • schematic symbol, PCB footprint and layout information for the ADSP-TS201 TigerSHARC Processor Evaluation Board
  • +ADSP-TS201S: FAQ
  • +CCES: FAQ
  • +cm40x: FAQ
  • +Command-line device programmer (cldp): FAQS
  • +Compiler: FAQ
  • +Connected Devices Virtual Conference: FAQS
  • +Disassembly Window: FAQ
  • +Enabling Product-Specific Push Notifications: FAQS
  • +ICE-1000: FAQ
  • +JEDEC J-STD-020: FAQ
  • +Misra rule checking: FAQ
  • +Nesting Interrupt: FAQ
  • +Power Domains: FAQ
  • +PROCESSORS AND DSP SUPPORT COMMUNITY: FAQS
  • +Questions 536 / VDK: FAQS
  • +RoHS-Compliant: FAQ
  • +Updating ICE-1000/2000 firmware with OpenOCD: FAQ
  • +VDSP-BLKFN-PC-FULL: FAQ
  • +VDSP-TS-PC-FULL: FAQ
  • +VDSP: FAQ
  • +VISUALAUDIO: FAQ

junction temperature on the ADSP-TS101 TigerSHARC Processor

Question

What is the maximum junction temperature on the ADSP-TS101 TigerSHARC
Processor?

Answer

The maximum case temperature (Tcase) for the ADSP-TS101 is 85C as shown in the
datasheet. In regards to the maximum junction temperature, this can be
calculated as follows:

Maximum power consumed by the core and I/O Calculation:
PD = Pint + Pext (Watts)

Maximum Case Temp Calculation:
Tcase (max) = Tambient + (PD * thetaCA)

As already stated, the value for Tcase (max) should be less than or equal to
85C (as defined in the data sheet).

where:

- Tambient is the air temperature in contact with the package of the device
- thetaCA is the case-to-ambient thermal resistance of the DSP package
- PD is the maximum total power consumed by the DSP (core and I/O)

Maximum Junction Temp Calculation:
Tjunction = Tcase (max) + (PD * thetaJC)

where:

- Tjunction is the junction temperature of the DSP
- Tcase is the maximum value for the case temperature of the DSP (should not
exceed 85C)
- thetaJC is the junction-to-case thermal resistance of the DSP

So depending on the airflow over the device and the package type (19x19mm or
27x27mm) you can use the above equations to determine Tjunction max for your
device in the system.

Tags: Processors & DSP 5FVQ1054 adsp-ts101s