Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Processors & DSP
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Processors & DSP
Processors & DSP
Documents Hooking up interrupts in VDK for programming with Blackfin processors
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADAU 1701: FAQ
  • +ADSP-21160M: FAQ
  • +ADSP-21363: FAQ
  • +ADSP-21368: FAQ
  • +ADSP-21369: FAQ
  • +ADSP-21469: FAQ
  • +ADSP-21489: FAQ
  • +ADSP-2160: FAQ
  • +ADSP-BF522: FAQ
  • +ADSP-BF531: FAQ
  • +ADSP-BF532: FAQ
  • +adsp-bf533: FAQ
  • +ADSP-BF534: FAQ
  • +ADSP-BF535: FAQ
  • +ADSP-BF536: FAQ
  • +ADSP-BF537: FAQ
  • +ADSP-BF538F: FAQ
  • +ADSP-BF539: FAQ
  • +ADSP-BF542: FAQ
  • +ADSP-BF544: FAQ
  • +ADSP-BF561: FAQ
  • +adsp-bf561: FAQS
  • +adsp-bf609: FAQS
  • +ADSP-BF60x: FAQ
  • +ADSP-BF70x: FAQ
  • +ADSP-CM408F: FAQ
  • +ADSP-SC58x: FAQ
  • +ADSP-TS001: FAQ
  • +ADSP-TS101S: FAQ
  • +ADSP-TS201S: FAQ
  • +CCES: FAQ
  • +cm40x: FAQ
  • +Command-line device programmer (cldp): FAQS
  • +Compiler: FAQ
  • +Connected Devices Virtual Conference: FAQS
  • +Disassembly Window: FAQ
  • +Enabling Product-Specific Push Notifications: FAQS
  • +ICE-1000: FAQ
  • +JEDEC J-STD-020: FAQ
  • +Misra rule checking: FAQ
  • +Nesting Interrupt: FAQ
  • +Power Domains: FAQ
  • +PROCESSORS AND DSP SUPPORT COMMUNITY: FAQS
  • +Questions 536 / VDK: FAQS
  • +RoHS-Compliant: FAQ
  • +Updating ICE-1000/2000 firmware with OpenOCD: FAQ
  • -VDSP-BLKFN-PC-FULL: FAQ
    • Does the ADDS-USB-ICE include any software (on disk)
    • Hooking up interrupts in VDK for programming with Blackfin processors
    • Problems with the license after PC change
    • restrictions when communicating with the EZ kit via USB with no ICE on a test drive
  • +VDSP-TS-PC-FULL: FAQ
  • +VDSP: FAQ
  • +VISUALAUDIO: FAQ

Hooking up interrupts in VDK for programming with Blackfin processors

Q 

How to map interrupt service routines if developing on VDK platform for
Blackfin processors?

 

A 

You can map the interrupt service routine by choosing one of the following ways:

1. Using VDK services: You can use the VDK services to hook an interrupt
service routine. Go to the Kernal tab in the project window and right click on
"Interrupts" and then click on "New Interrupt" and add your code in the
generated C++/C/asm source file.

2. Just as standalone applications: One can map interrupts just as you
implement it in the standalone program. Please refer to the Program Sequencer
chapter (Chapter 4) of the ADSP-BF53x/56x processor programming reference
manual for more details or follow any
of the example included in the VisualDSP++ program folder (for e.g. C:\Program
Files\Analog Devices\VisualDSP 4.5\Blackfin\Examples\ADSP-BF533 EZ-Kit
Lite\Video Input (C) to hook an interrupt).

Also, be careful while using the IMASK register in VDK based applications.
Modify IMASK register in
critical regions only (disabling all interupts in the system).

3. Using System services: Using the system services API's (adi_int_CECHook())
or if implementing using the device driver model than one can use the Callback
service.

Tags: vdsp-blkfn-pc-full
  • Share
  • History
  • More