Power Management Fundamentals II Session 5: Deeper Look into Power Protection

    When is the best time to discover your power circuit needs protection? Let's explore the use of some input protection and control options like ideal diodes...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

     

    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

    Latest Blogs

    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
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
Processors & DSP
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Processors & DSP
Processors & DSP
Documents How do I validate SPI on my newly designed board based on ADSP-SC58x/ADSP-2158x processors?
  • Forums
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADAU 1701: FAQ
  • +ADSP-21160M: FAQ
  • +ADSP-21363: FAQ
  • +ADSP-21368: FAQ
  • +ADSP-21369: FAQ
  • +ADSP-21469: FAQ
  • +ADSP-21489: FAQ
  • +ADSP-2160: FAQ
  • +ADSP-BF522: FAQ
  • +ADSP-BF531: FAQ
  • +ADSP-BF532: FAQ
  • +adsp-bf533: FAQ
  • +ADSP-BF534: FAQ
  • +ADSP-BF535: FAQ
  • +ADSP-BF536: FAQ
  • +ADSP-BF537: FAQ
  • +ADSP-BF538F: FAQ
  • +ADSP-BF539: FAQ
  • +ADSP-BF542: FAQ
  • +ADSP-BF544: FAQ
  • +ADSP-BF561: FAQ
  • +adsp-bf561: FAQS
  • +adsp-bf609: FAQS
  • +ADSP-BF60x: FAQ
  • +ADSP-BF70x: FAQ
  • +ADSP-CM408F: FAQ
  • -ADSP-SC58x: FAQ
    • How do I validate SPI on my newly designed board based on ADSP-SC58x/ADSP-2158x processors?
    • How do I validate the SPORT on my newly designed board based on ADSP-SC58x/ADSP-2158x processors?
    • How do I validate the UART on my newly designed board based on ADSP-SC58x/ADSP-2158x processors?
    • How do I validate TWI on my newly designed board based on ADSP-SC58x/ADSP-2158x processors?
  • +ADSP-TS001: FAQ
  • +ADSP-TS101S: FAQ
  • +ADSP-TS201S: FAQ
  • +CCES: FAQ
  • +cm40x: FAQ
  • +Command-line device programmer (cldp): FAQS
  • +Compiler: FAQ
  • +Connected Devices Virtual Conference: FAQS
  • +Disassembly Window: FAQ
  • +Enabling Product-Specific Push Notifications: FAQS
  • +ICE-1000: FAQ
  • +JEDEC J-STD-020: FAQ
  • +Misra rule checking: FAQ
  • +Nesting Interrupt: FAQ
  • +Power Domains: FAQ
  • +PROCESSORS AND DSP SUPPORT COMMUNITY: FAQS
  • +Questions 536 / VDK: FAQS
  • +RoHS-Compliant: FAQ
  • +Updating ICE-1000/2000 firmware with OpenOCD: FAQ
  • +VDSP-BLKFN-PC-FULL: FAQ
  • +VDSP-TS-PC-FULL: FAQ
  • +VDSP: FAQ
  • +VISUALAUDIO: FAQ

How do I validate SPI on my newly designed board based on ADSP-SC58x/ADSP-2158x processors?

The attached code can be used as a reference to test SPI connections on newly designed board with ADSP SC58x/ ADSP-2158x processors.

The code does the following:

  • This code intends to test data transfer between the two SPI modules in auto-buffered DMA mode.
  • The SPI is configured in a half-duplex configuration with one SPI as the master transmitter and the other SPI as the slave receiver.
  • The code tests for two types of data patterns:
    • Fixed data pattern as 0xAA: This is to check whether the SPI transmit data comes out well when the SPI MOSI channel is probed using a scope.
    • Random data: This is to make sure that the transmitted data is received properly when it is received by the SPI configured as the slave receiver.
  • Appropriate connections should be made externally based on the TX and RX choice. For example, if SPI0 is configured as the master transmitter while SPI1 is configured as the slave receiver. In this case, the connections need to be made as follows:
    • SPI0_CLK <--> SPI1_CLK
    • SPI0_MOSI <--> SPI1_MOSI
    • SPI0_MISO <--> SPI1_MISO
    • SPI0_SEL (Master) <--> SPI1_SS (Slave)
  • It is recommended to disable cache before executing this code.

How to modify the code for customized system requirements:

  • The existing code provides the flexibility to configure any of the SPIs as the transmitter and the receiver after appropriate changes in the macros.
  • The existing code uses SPI0 is configured as the master transmitter while SPI1 is configured as the slave receiver. The SPI configuration can be modified to use any other combination of SPIs.
  • Various configuration settings for SPI have also been defined in the macros.

How to test that the code works?

  • To make sure that the SPI signals are coming out on the pins as expected, probe the SPI master clock, MOSI pins. To make sure that a known data (e.g. 0xAA as byte of the frame in this case) is transferred for easy probing, use the definition “Fixed_data”(see below screenshot)

The below screenshot shows how the SPI CLK and MOSI signals should look like

  • For a quick sanity check that the SPI slave receiver is able to receive the data as expected, one can look at compare the transmit and receive data (in random data format) by looking at the CCES memory window as shown in the screenshot below:

Attachments:
SPI_Sample_Auto_Core1.zip
Tags: processors adsp-2158x ADSP SC58x spi
  • Share
  • History
  • More