Disassembly windows display disassembled instructions and symbolic information, which is useful for temporarily modifying the code to test a change or to view code when no source is available. The Disassembly window allows you to examine the assembly code generated by the C/C++ compiler. Symbolic information includes alphanumeric characters representing values and addresses.You can perform the following in the view:
• Setting breakpoints at the start of any assembly instruction • Enabling or disabling breakpoints and setting their properties• Stepping through disassembled instructions • Jumping to specific instructions, symbols, or expressions • Temporarily modifying code in order to test a change or view code when no source is available
To explore the Disassembly view:For CCES: Choose Window > Show View > Other > Debug > Disassembly and click OK.For VDSP: By default,a Disassembly window appears when you open a new session.If not you can choose View > Debug windows > Disassembly
Please refer the below help path for more information on Disassembly windows:
If you are using CCES:CCES help > Help contents > CrossCore Embedded Studio 2.6.0 > Integrated Development Environment > Navigating Within the IDE > Views > Debug > Disassembly View
If you are using VisualDSP++:VisualDSP help > contents > Graphical Environment > IDDE > Environment >Debug Windows > Disassembly Windows